Skip to main content
MLang.7
Associate III
Jul 18, 2022 8:53 AM UTC
Question

Program generated by TouchGFX crashes after changing the .ioc file

Good morning,

currently I am experimenting with a STM32H735G-DK demo board. I started with generating a simple Button for toggeling an LED in Touch GFX. Then I opened the project in the STM32CubeIDE and changed a GPIO pin. After compiling the program, the controller immediately crashes and the MemManage_Handler is invoked.

I tried to verify the problem and repeated the steps with a new project. In this case, I just ran the configuration tool without making any changes which showed the same result. So I think there is a problem with the configuration file ***/or settings.

Unfortunately I am not able to find the cause for crashing, so I do rely on a working configuration for now.

This topic has been closed for replies.

1 reply

Yoann KLEIN
ST Employee
Jul 20, 2022 7:12 AM UTC

Hello @MLang.7​ ,

Could you please share your project, to make it easier for us to reproduce the issue ?

Thank you by advance.

/Yoann

Yoann KLEINST Software Developer | TouchGFX