Skip to main content
ddelt.1
Associate
February 5, 2020
Question

Problems of sources building within STM32cubeIDE

Here is my problem:

I create a STM32cube IDE project by including an additionnal software named TouchGFX . I generate the project so that it gets

with the discovery 32F469 NI card...and a windows message appears which is following: " These IPs still have some not configured or wrong parameters values [STMicroelectronics

X-CUBE-TOUCHGFX 4.13.0.

The build of the project gives some errors identified in the OSwrappers and TouchGFXconfiguration .cpp

This topic has been closed for replies.

1 reply

Martin KJELDSEN
Principal III
March 31, 2020

Can you please post the errors here?

"These IPs still have..." appears when you have "warnings" or unfulfilled dependencenies in TouchGFX Generator or other places in CubeMX

E.g. If CRC is not enabled, you'll get an error.

/Martin