Skip to main content
SKILA
Associate III
January 12, 2021
Question

Problems after updating to CubeMX 6.1 and Touchgfx 4.16

Hello,

I have recently decided to try upgrading a project I have originally generated using CubeMx 5.6 and designed using TouchGFX 4.13 to CubeMx 6.1 and TouchGFX 4.16. After some teething problems, I have managed to get it working and running on my custom STM32F7 board. The only problem is that there are about 2 images that when shown on the LCD screen come up with distorted colours.

Any idea what might be causing this?

RegardsSamer

This topic has been closed for replies.

3 replies

Romain DIELEMAN
ST Employee
January 12, 2021

Hum that is interesting. Is it only 2 images you have that are being distorted ? It does not happen for the other ones ? Does it also distort boxes of different colors ?

Could you share the color depth/ image format / using alpha or not /etc ?

/Romain

SKILA
SKILAAuthor
Associate III
January 12, 2021

Yes, only two images have this effect. Everything else is absolutely fine. Boxes, circles etc are all good.

This is extracted from the generated image files

// 4.16.0 0x9291f5ce D2 R1 FL8_RGB565 U565 N0 SExtFlashSection EExtFlashSection

By the way, I compared the generated files of 4.13 and 4.16 and they are the same. I guess it has something to do with rendering these images rather than the generation.

Samer

SKILA
SKILAAuthor
Associate III
January 12, 2021

@Romain DIELEMAN​ I have managed to sort it out by manually setting the image format of these two images to L8_ARGB8888. It was previously set to the default which is L8_RGB565 / L8_ARGB8888. To be honest, I don't know the exact criteria that define an image to be opaque or non-opaque (transparency?) my guess is that in touchgfx 4.13 it chose the non-opaque image format for these two files while 4.16 chose the opaque format.

I know I have a solution but still very interested in knowing why this has happened...