Skip to main content
MEige
Associate II
Mar 24, 2026 12:48 PM UTC
Solved

Problem with Touchgfx "Program and Run Target" ->STM32N6570-DK

Hello

"Program and Run Target" stops with some Messages (Small Test Prog.)

"Program All":

 -------------------------------------------------------------------
 STM32CubeProgrammer v2.22.0 
 -------------------------------------------------------------------

 Memory Programming ...
 File : STM32N6570-DK_FSBL-trusted.bin
 Size : 32.63 KB 
 Address : 0x70000000 
 
 Erasing memory corresponding to segment 0:
 Erasing external memory sector 0
 Error: failed to erase memory
 
 Error: failed to erase memory
 c:/TouchGFXProjects/MyApplication_5/gcc/include/flash_sections_int_ext.mk:18: recipe for target '_fsblflash_' failed
 make[2]: *** [_fsblflash_] Error 1
 makefile_fsbl:45: recipe for target 'flash' failed
 make[1]: *** [flash] Error 2
 ../../gcc/Makefile:8: recipe for target 'flash' failed
 make: *** [flash] Error 2
 Failed

 

"Program Internal Flash":

 Memory Programming ...
 File : STM32N6570-DK_Appli-trusted.bin
 Size : 345.22 KB 
 Address : 0x70100000 
 
 Erasing memory corresponding to segment 0:
 Erasing external memory sectors [16 21]
 Error: failed to erase memory 
 
 Error: failed to erase memory
 c:/TouchGFXProjects/MyApplication_5/gcc/include/flash_sections_int_ext.mk:12: recipe for target '_intflash_' failed
 make[2]: *** [_intflash_] Error 1
 makefile_appli:55: recipe for target 'intflash' failed
 make[1]: *** [intflash] Error 2
 ../../gcc/Makefile:12: recipe for target 'intflash' failed
 make: *** [intflash] Error 2
 Failed
 Failed

 

A second "Program and Run Target"  is necessary to correctly programm the STM32N6. To start the Prog.  a Cold Boot (Power off/of) is necessary.

PC: Standard PC Win 10

BTW: Some Demos are making Problems also. The "Coffee Machine Demo" stops with

 

 make (e=206): Der Dateiname oder die Erweiterung ist zu lang.
 
 make[3]: *** [Appli/TouchGFX/build/bin/target.elf] Error 206
 make[2]: *** [generate_assets] Error 2
 Failed
 ../../gcc/Makefile:8: recipe for target 'all' failed
 make[1]: *** [all] Error 2
 make: *** [all] Error 2
 Failed

Der Dateiname oder die Erweiterung ist zu lang = Filename or Extension is to long.

Marc

    MEige
    MEigeBest answer
    Associate II
    Mar 24, 2026 1:52 PM UTC

    Edit:

    I managed to get the Coffee demo running. I changed OS from FreeRTOS to ThreadX.

    1 reply

    MEige
    MEigeAuthorBest answer
    Associate II
    Mar 24, 2026 1:52 PM UTC

    Edit:

    I managed to get the Coffee demo running. I changed OS from FreeRTOS to ThreadX.