Skip to main content
Vlaty.1
Associate III
March 1, 2021
Solved

Problem with STM32F764

Good afternoon, I'm trying to use STM32F746ZGTx LQFTP144 for a railway scoreboard.(Commuter train schedule) I have a problem. I ran a BSD project on the Nucleo-144 STM32F746 board from the STM32746G_DISCOVERY examples. I commented out everything except the LCD. Display_Demo Description() Using the oscilloscope, I found that the following outputs of the controller are active.

PD9

PG12 LCD_B1

PG15

PG0

PD0

PD1

PH0 OSC

PF2

PH1 OSC

PE4 LCD_B0

PA14 SW

PE14 LCD_CLK

PF13 

PD10 LCD_B3

PD15

PE7

PE8

PF4

PF5

PD8

This list does not match the description of stm32f745ie. pdf and CubeMX. I hope you can help me figure out which controller pins are actually used to control the LCD. Sincerely, Alexander.

This topic has been closed for replies.
Mike_ST
Mike_STBest answer
ST Technical Moderator
March 1, 2021

The stm32f7xx_hal_msp.c file is not inside the STM32F7xx_HAL_Driver folder, this is a file that you have to edit depending of your project.

look example here :

C:\Users\$USER\STM32Cube_FW_F7_V1.16.1\Projects\STM32746G-Discovery\Examples\LTDC\LTDC_Display_1Layer\Src

It can also be generated by the STM32CubeMX, if you generate init code with it.

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. 

11 replies

Mike_ST
ST Technical Moderator
March 1, 2021

Hello,

What does not match, precisely ?

The main.c file doesn't show any pin configuration.

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. 
Vlaty.1
Vlaty.1Author
Associate III
March 1, 2021
It from C:\Users\user\STM32Cube\Repository\STM32Cube_FW_F7_V1.11.0\Projects\STM32746G-Discovery\Examples пн, 1 мар. 2021 г. в 12:28, ST Community :
Mike_ST
ST Technical Moderator
March 1, 2021

"This list does not match the description of stm32f745ie. pdf and CubeMX"

What pin exactly does not match your expection ?

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. 
Mike_ST
ST Technical Moderator
March 1, 2021

---

Wrong post

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. 
Vlaty.1
Vlaty.1Author
Associate III
March 1, 2021
The "Connector" circuit contains the expected signals required to control the liquid crystal display.(According to your description) But in fact, these signals are not present in STM32F746 Nucleo-144. But they are on the list I sent you. It seems that somewhere in the board or in the controller there is a mismatch between the pins and additional functions (LCD) Sincerely, Alexander. пн, 1 мар. 2021 г. в 13:29, ST Community :
Mike_ST
ST Technical Moderator
March 1, 2021

The LTDC examples you are mentionning, are for the discovery board that have a BGA216 package and which have obviously more pin than a LQFP 144 package.

You probably have to adapt the stm32f7xx_hal_msp.c to remap the LTDC pins definition to match the LFQP144 pinout description, if this is possible.

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. 
Vlaty.1
Vlaty.1Author
Associate III
March 1, 2021
I do not have the stm32f7xx_hall_msp.c file in the STM32F7xx_HAL_Driver library, but if you send me instructions, I can probably solve the problem. Sincerely, Alexander. пн, 1 мар. 2021 г. в 14:17, ST Community :
Mike_ST
Mike_STBest answer
ST Technical Moderator
March 1, 2021

The stm32f7xx_hal_msp.c file is not inside the STM32F7xx_HAL_Driver folder, this is a file that you have to edit depending of your project.

look example here :

C:\Users\$USER\STM32Cube_FW_F7_V1.16.1\Projects\STM32746G-Discovery\Examples\LTDC\LTDC_Display_1Layer\Src

It can also be generated by the STM32CubeMX, if you generate init code with it.

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.