Skip to main content
Alberto1
Associate II
Feb 14, 2023 11:16 AM UTC
Question

Problem with "Run Target" on TouchGFX Designer: target/gcc/Makefile: No such file or directory

I state that I have already seen this problem within the community, but I was unable to solve my problem.

I'm reading the TouchGFX Documentation to be able to develop an application: I followed the instructions in "Code Structure" with the simple example provided.

If I go to simulation, everything is ok.

If instead I try to execute "Run Target", I am returned:

compile

make -f target/gcc/Makefile -j8

make: target/gcc/Makefile: No such file or directory

make: *** No rule to make target 'target/gcc/Makefile'. Stop.

Failed

Checking in "Config" of the TouchGFX Designer, I noticed that the lines "Compile Target Command" and "Flash Target Command" are not compiled.

I entered "make -f target/gcc/Makefile -j8" and "make -f target/gcc/Makefile -j10 flash" respectively.

The result doesn't change.

I also noticed that while the gcc folder is present in the "simulator" folder, it is not present in the "target" folder.

How can I solve the problem? What does it depend on?

Thank you in advance.

Alberto

This topic has been closed for replies.

11 replies

Alberto1
Alberto1Author
Associate II
Feb 14, 2023 2:40 PM UTC

After a deep searching I discovered that the "gcc" directory in the root of the example, there wasn't.

Now the question is: how can I procede?

Do I have to insert it or, as I think, should "the system" (CubeMX, CubeIde, TouchGfx..) create it autonomously?

Thanks

Yoann KLEIN
ST Employee
Feb 14, 2023 2:48 PM UTC

Hello @Alberto​,

Did you start your project from a TouchGFX Board setup in TouchGFXDesigner ?

If yes, then the gcc folder is already included inside the project and you can directly run your project on target.

/Yoann

Yoann KLEINST Software Developer | TouchGFX
Alberto1
Alberto1Author
Associate II
Feb 14, 2023 2:57 PM UTC

Hello @Yoann KLEIN​ 

First of all thanks for your reply.

I use a STM32H7B3I-DK and I started from CubeMX where I defined the pinout for supporting the onboard display.

I genereted code and I use CubeIde to follow the example describe in the documentation.

Aftre I use TouchGFX to insert the 2 widget (as describe in documentation).

MM..1
Super User
Feb 14, 2023 6:43 PM UTC

Your steps is OK, but MX created projects dont enable run on target (not filled),

run to target here is possible only in IDE selected in MX. (IDE/KEIL/IAR ...)

In TouchGFX is enabled only generate code (required step after gui change) and simulate partialy

After generate close touchgfx or switch to IDE opened ...

Alberto1
Alberto1Author
Associate II
Feb 15, 2023 8:28 AM UTC

Hi!

@Romain DIELEMAN​ @MM..1​ 

Thanks again.

This could be quite a problem.

I have no experience with "makefile" and "linker script"...and I have to develop a firmware on a custom board.

However, I managed to eliminate the error messages (of the Run Target), by modifying a "makefile" of an example, as you suggested.

Now the program is downloaded in my board, but nothing is visible.

Using the simulator, however, you see the graphical interface created.

So, either something is wrong in the "makefile"/"linker script" or the code generated by TouchGfxDesigner is incorrect.

In addition, even going into debug on the CubeIde I get the same result: nothing is visible. ...so I don't know how to proceed.

Summary, from what I understand, correct me if I'm wrong, I could (after creating the project with CubeMX and CubeIde...) switch to TouchGFX Designer, create the user interface and then via CubeIde run the program and see the UI interface. Right?

Alberto

Romain DIELEMAN
ST Employee
Feb 15, 2023 8:36 AM UTC

Hello,

​

Yes you are right it will be easier to just design your UI in TouchGFX Designer and then run the program via STM32CubeIDE.

The fact that you currently see nothing could come from many things though :grinning_face_with_sweat: I would recommend the test in this article to see if you have correctly enabled your display first.

/Romain

Alberto1
Alberto1Author
Associate II
Feb 15, 2023 8:56 AM UTC

Hi!

Yes, in fact it can be a bit of everything...:D

I read the article and the card (STM32H7B3I-DK) was working fine.

Then, perhaps, by modifying the project from CubeMX to support TouchGFX, some setting has been lost...

I'll do some tests and check.

Anyway, thanks again for everything.

Alberto