Associate III
Feb 21, 2020 12:11 PM UTC
Question
Powerup problem TouchGFX with STM32F746
- 1 reply
- 641 views
I am working with touchGFX on the custom board with STM32F746. A 2-screen touchgfx application works without problems when debugging with cubeMXIDE. It doesn't work when I remove the STlink and powerup it. I put a heartbeat to understand that the processor is working. If I comment out the line MX_TouchGFX_Init (), then heartbeat works after powerup. I am using QUADSPI bank1 and SDRAM bank 2. FreeRtos is not used.