Skip to main content
BParh.1
Senior III
June 4, 2021
Question

Potential Bug? : Build Error when using TouchGFX and MSVC Simulator .sln interchangeably

Steps:

  1. Use TouchGFX Designer to setup some GUI e.g. dynamic graph and generate the code then run simulation, make sure it is ok
  2. Open the MSVC simulator. Made some modification on the code or add additional cpp/hpp file into project. Build in MSVC make sure it is ok
  3. Switch again to TouchGFX Designer which might prompt you to accept external change. Click ok then generate the code and run simulator again -> build fail.

I notice in the code suddently the dynamic graph of the element area and element line instance were gone. As work around I needed to delete and create again the elemenet area and element line in TouchGFX Designer.

Following is the build error log snippet:

Run Simulator
 Generate
 Wrote generated/gui_generated/include/gui_generated/containers/CurveViewBase.hpp
 Wrote generated/gui_generated/src/containers/CurveViewBase.cpp
 Done
 Generate Assets
 make -f simulator/gcc/Makefile assets -j8
 Reading ./application.config
 Done
 Post Generate
 touchgfx update_project --project-file=simulator/msvs/Application.vcxproj
 Done
 Post Generate Target
 touchgfx update_project --project-file=../STM32F769I_DISCO.ioc --platform=m7
 Done
 Compile
 make -f simulator/gcc/Makefile -j8
 Reading ./application.config
 Compiling gui/src/home_screen/HomeView.cpp
 Compiling gui/src/home_screen/HomePresenter.cpp
 Compiling gui/src/containers/CurveView.cpp
 Compiling gui/src/model/SystemIfc.cpp
 Compiling gui/src/model/Model.cpp
 Compiling generated/gui_generated/src/home_screen/HomeViewBase.cpp
 Compiling generated/gui_generated/src/containers/CurveViewBase.cpp
 Compiling generated/gui_generated/src/common/FrontendApplicationBase.cpp
 Compiling generated/simulator/src/mainBase.cpp
 Compiling simulator/main.cpp
 In file included from gui/include/gui/containers/CurveView.hpp:4:0,
 from gui/include/gui/home_screen/HomeView.hpp:4,
 from gui/src/home_screen/HomeView.cpp:1:
 generated/gui_generated/include/gui_generated/containers/CurveViewBase.hpp:59:15: error: using-declaration for non-member at class scope
 touchgfx::GraphElementArea ;
 ^~~~~~~~~~~~~~~~
 generated/gui_generated/include/gui_generated/containers/CurveViewBase.hpp:61:15: error: using-declaration for non-member at class scope
 touchgfx::GraphElementLine ;
 ^~~~~~~~~~~~~~~~

This topic has been closed for replies.

5 replies

MM..1
Super User
June 4, 2021

Maybe in point 2 you edit some files , that is generated and isnt designed to edit. Place your code in GUI files not in generated... Generated files is always overwrited in point 3

BParh.1
BParh.1Author
Senior III
June 5, 2021

Thank you @MM..1​  for the response but I did put it in gui/ folder. I am well aware not to touch the generated code part or folder :)

BParh.1
BParh.1Author
Senior III
June 13, 2021

Any update to this issue please? This is getting annoying as I have to do work around to resolve the issue on regular basis

LKade.1
Associate II
January 26, 2022

Hi @BParh.1​ 

Were you to able to solve the issue, has i am facing the same issue for gernerated GUI.

if you have a solution for the above please do guide me also.

Thanks

With Regards

Lakshminarayana

BParh.1
BParh.1Author
Senior III
January 27, 2022

Hi @LKade.1​ ,

The issue resolve but I did not how :). I just made series of seems unrelated changes, but these two probably the most likely resolve it:

  1. Upgrade my TouchGFX Designer from v4.16 to v.47. May be just consider upgrade to latest, I think there is newer version.
  2. I change the dynamic graph widget from custom container to directly insert it in screen level. Or vice versa, I forgot which one,maybe you could try both.

Please try and let me know how it goes, all the best!