Skip to main content
Associate III
Aug 30, 2025 3:54 AM UTC
Question

partial bitmap copy in Touchgfx

Hello everyone:

I came to a need,that I need to copy part of a dynamic Bitmap to another postion of the same bitmap.I current use a for loop and memcpy func,It works but cost 4ms each run.How can I use touchgfx's blockCopy functions to do this? as DMA2D was already enabled.

000.png

This topic has been closed for replies.

3 replies

ambAuthor
Associate III
Aug 30, 2025 3:57 AM UTC

I found blitCopy() func in HAL.hpp,but it seems it only use to FRAMEBUFFER.

Flemming Gram CHRISTENSEN
ST Employee
Sep 1, 2025 1:11 PM UTC

Hi amb

We don't have that operation, but I think you can make one.

first call HAL::lockFrameBuffer. This will wait for the DMA to finish all operations.

call unlockFrameBuffer also.

Now, DMA2D is idle and we can use it.

Two ways:

Go to your CubeFW for the board (or another board with DMA2D and display), find the DMA2D examples.

For F746Discovery, for example this:
STM32Cube_FW_F7_V1.17.0/Projects/STM32746G-Discovery/Examples/DMA2D/DMA2D_MemToMemWithPFC/Src/

Use this code to setup DMA2D and start it.

Second:

Take the code from STM32DMA::setupDataCopy. Find the default case, marked with /* BLIT_OP_COPY */.

Use this to make a specific function for your need.

 

Let me know if you have questions.

 

Note, using DMA2D within TouchGFX requires caution. It is not recommended, unless you need to.

 

 

ambAuthor
Associate III
Sep 1, 2025 1:41 PM UTC

Hello:@Flemming Gram CHRISTENSEN 

Thanks for your reply.I will try it.

And I have another question: the touchgfx framebuffer is RGB565,Can I make a dynamic bitmap of ARGB8888?  I made one by cacheable container and display the dynamic bitmap by a texturemapper but no image came out. but if I change bitmap type to rgb565,the image can be seen. There is enough  cache,I confirm the dynamic bitmap is created successfully on both type.