Skip to main content
Senior II
Sep 19, 2024 4:51 AM UTC
Solved

parallel processing using ili9488 display and microcontroller

i have created a user interface using touchgfx when i go to the second page sine wave has to be generated and parallelly display has to work is it possible to do this using controller or should i go for mpu
    This topic has been closed for replies.
    SharanBest answer
    Senior II
    Oct 3, 2024 5:25 AM UTC

    hi                                                                                                                                                                                          i am working on stm32mp157d-dk1 now so now i will be generating sine wave using the mpu instead of microcontroller and can we access the adc and dac using arm cortex a7 and if possible how to do it?

    15 replies

    mƎALLEm
    ST Technical Moderator
    Sep 19, 2024 7:59 AM UTC

    Hello,


    @Sharan wrote:
    i have created a user interface using touchgfx when i go to the second page sine wave has to be generated and parallelly display has to work 

    This statement is not clear. Could you please give more details about your issue, request?

    To give better visibility on the answered topics, please click "Best answer" on the reply which solved your issue or answered your question.
    SharanAuthor
    Senior II
    Sep 19, 2024 8:08 AM UTC

    i have purchased the STM32MP157D-DK1 mpu and i have ili9488 display can i do parallel processing, that is display has to work and parallelly signal generation has to happen or is it possible using microcontroller 

    GaetanGodart
    ST Employee
    Sep 20, 2024 7:23 AM UTC

    Hello @Sharan ,

     

    1. You can indeed create a GUI design using TouchGFX
    2. You an control a display with ili9488 driver, you will have to follow this guide : board-introduction 
    3. You can generate a sine wave (either from hardware or software), then you can send it to your GUI using the MVP design : model-view-presenter-design-pattern 

     

    I hope this helps! :smiling_face_with_smiling_eyes:
    If this comment or another one answers your questions, I invite you to select that comment as "best answer".

     

    Regards,

    Gaetan GodartSoftware engineer at ST (TouchGFX)
    SharanAuthor
    Senior II
    Sep 20, 2024 7:38 AM UTC

    using mvp model i was able to generate sine wave but i required 10k i only got 3k

    GaetanGodart
    ST Employee
    Sep 23, 2024 8:13 AM UTC

    What do you mean by "10k" and "3k"?

    You need 10 000 sine wave at the same time?

    Gaetan GodartSoftware engineer at ST (TouchGFX)
    SharanAuthor
    Senior II
    Sep 23, 2024 10:46 AM UTC

    the frequency of sine wave is 10,000hz which means 10000 sine waves per second

    mƎALLEm
    ST Technical Moderator
    Sep 23, 2024 10:51 AM UTC

    @Sharan wrote:

    the frequency of sine wave is 10,000hz which means 10000 sine waves per second


    You mean 10000 samples of the sine wave per second.

    To give better visibility on the answered topics, please click "Best answer" on the reply which solved your issue or answered your question.
    Andrew Neil
    Super User
    Oct 3, 2024 11:45 AM UTC
    A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.