Skip to main content
PFlor.2
Senior II
Jun 25, 2023 3:17 AM UTC
Question

Override flexButtonCallbackHandler() or buttonCallbackHandler()

I have several flex and nonflex buttons on a screen and wanted to be able to call a beeper function with any button press.  So I thought I could override the callback handler for button and flexButton to do this.  Is this not possible since they are private in the base class?  I'm used to C and not very familiar with C++ classes and inheritance.

This topic has been closed for replies.

1 reply

MM..1
Super User
Jun 25, 2023 6:23 AM UTC

If your design is based on touch only try implement beeper in touch handler. 

Other workaround is create thread for beeper and on every callback send to queue message beep...