Skip to main content
SPrak.4
Associate II
Oct 2, 2019 10:54 AM UTC
Question

ov9655 output format analysis

I capture an image using the ov9655 camera module. The selected the image format as rgb565. The image captured is getting captured clearly (as i can see it on the lcd). As a next step, I wanted to analyse how the image is stored in the camera buffer.

The size of buffe is 320 and consits of 16 bit 320 HEX values. I want to convert this to rgb565 and check if I get the correct pixel color. Could anyone help me with this?

I am confused as the camera datasheet talks something about the Bayer pattern for output patter which seems to be different from the arrangement of rgb565 format

This topic has been closed for replies.