Skip to main content
franck23
Associate III
Jan 6, 2021 7:21 PM UTC
Question

Offset X axis in histogram

Hi,

When using the histogram, the first bar is by default centered on 0 which makes it only half visible:

0693W000006Hl6OQAS.png 

The bars offset can be increased, moving them to the right. However, I could not find a way to shift the X-axis so the X labeling is no more in the center of the bars:

0693W000006Hl6TQAS.png 

There is also the possibility to set the left and right padding, but in this case, the horizontal grid lines do not extend in the padding:

0693W000006Hl6YQAS.png 

Is there any way to have all bars fully visible, the X-axis labels centered with the bars, and the horizontal grid lines?

Thanks for any help,

Franck.

Edit: Re-attach pictures

This topic has been closed for replies.