Skip to main content
Associate
Feb 7, 2025 9:03 PM UTC
Solved

NUCLEO-U5A5ZJ-Q with Riverdi RVA35HI

Hi,

I am currently waiting for the Riverdi RVA35HI display to arrive at my door.
On the website (3.5” STM32 Nucleo 144 Display Kit - Riverdi) it says the display is compatible with NUCLEO-H563ZI and NUCLEO-U575ZI-Q and I have already seen the Nucleo-U575ZI + RVA35HI integration in TouchGFX.

Since I have a NUCLEO-U5A5ZJ-Q at home and it is quite similar to the NUCLEO-U575ZI-Q, can I use the display with the integration in TouchGFX for my MCU or do I have to be aware of anything?

Thanks & best regards
Zarzi

This topic has been closed for replies.
LouisBBest answer
ST Employee
Feb 10, 2025 9:31 AM UTC

The simple answer is no that's not possible, TBS are made specifically for one board.

The more complex answer, If you want to use a board that doesnt have a TBS, you need to configure everything manually (In CubeMX)  : Board Bring Up Introduction | TouchGFX Documentation but that's an hard task.

Louis BOUDOST Software Engineer | TouchGFX

3 replies

ST Employee
Feb 10, 2025 8:11 AM UTC

Hello @Zarzi ,

 

The NUCLEO-U5A5ZJ-Q doesn't have a out-of-the-box TBS, have you already used it for TouchGFX ?

 

Best regards,

Louis BOUDOST Software Engineer | TouchGFX
ZarziAuthor
Associate
Feb 10, 2025 8:33 AM UTC

Hi @LouisB,

 

Thank you for your answer.

No I did not do any TouchGFX project before. Can I use the TBS of the NUCLEO-U575ZI-Q x Riverdi RVA35HI, generate the code and copy the files and pin assignments to my existing NUCLEO-U5A5ZJ-Q project or how would you suggest to make this work?

 

Thanks & best regards

Zarzi

LouisBBest answer
ST Employee
Feb 10, 2025 9:31 AM UTC

The simple answer is no that's not possible, TBS are made specifically for one board.

The more complex answer, If you want to use a board that doesnt have a TBS, you need to configure everything manually (In CubeMX)  : Board Bring Up Introduction | TouchGFX Documentation but that's an hard task.

Louis BOUDOST Software Engineer | TouchGFX