Skip to main content
BTeof.1
Visitor II
Sep 12, 2022 4:44 PM UTC
Question

nucleo-g071rb + example touchGfx designer 4.1.16

I’m trying to run the example of touchgfx stm32g071 nucleo demo, but when I import to stm32ide and debug, the program never returns from the function "void tick" in " HAL::getInstance()->backPorchExited() or do I need to change the code somewhere?

thank you.

This topic has been closed for replies.

1 reply

Yoann KLEIN
ST Employee
Sep 13, 2022 7:09 AM UTC

Hello @BTeof.1​ ,

If I understand correctly, you are using TouchGFX 4.16 ?

If yes, could you please upgrade to 4.20 and see if there is still compilation errors ?

Thank you,

/Yoann

Yoann KLEINST Software Developer | TouchGFX