Skip to main content
TCygan
Associate II
December 11, 2020
Question

Noob question. I have STM32H7B3I-DK and need to connect and grab info from the internet. Need a sample project.

So I'm new to this development.  I have STM32H7B3I-DK and need to connect to wifi/Internet and grab some data. I've experimented with TouchGFX Designer and there are templates that I like, especially the lens widget. Here are my questions:

  1. Is there a sample project that I can use?
  2. Would this entail the use of TouchGFX and some other software? Perhaps CubeIDE?
  3. Is there a good pdf or video on how to use TouchGFX with CubeIDE?

Thank you!!

**FYI; I'm running TouchGRX 4.15.0, CubeIDE 1.5.0, CubeProgrammer 2.5

This topic has been closed for replies.

1 reply

ST Technical Moderator
January 9, 2021

Hello @TCygan​ ,

You can follow the TouchGFX getting started and create your project from TouchGFX Designer with the right application template, then launch STM32CubeIDE and open the project generated (in the directory C:\TouchGFXProjects)

You have also the TouchGFX tutorials and TouchGFX MOOC to start your project,

Imen

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Thanks