Skip to main content
Zu_it
Associate II
July 27, 2021
Solved

No rule to make target when I remove images

Hello,

I am doing these steps:

  • I made a new project
  • added a button with a random image and a text label
  • compiled and executed
  • opened the project in stm32cubeide
  • added into the project some libraries that I am using to read sensors
  • compiled and executed on the target with stm32cubeide
  • Removed the button compiled and executed with stm32cubeide [ERROR: make: *** No rule to make target '../Application/User/generated/image_Dark_Slider_Vertical_Medium_Slider3_Vertical_fill.cpp', needed by 'Application/User/generated/image_Dark_Slider_Vertical_Medium_Slider3_Vertical_fill.o'. Stop.]
  • but if I compile with touchgfx to the target, it works without errors.

Touchgfx 4.17.0

stm32cubeide Version: 1.6.1

How I can dig into the problem?

I also tried to regenerate the code and update the ioc file.

Thanks

This topic has been closed for replies.
AAdam.2
AAdam.2Best answer
Visitor II
November 4, 2021

Hi Roman,

Thank you for the feedback. Well after I wrote that I figured.. HEY!!, I'm not going to let this thing beat me, and I better figure it out incase it happens again (which is a pretty safe bet probably). All I ended up having to do was go into application/user/generated/ and delete the .cpp files that were associated with the removed images from tGFX designer. They were obvious because then were marked with a '!'. The files were completed empty, but still in the file system.

Is there a way to "clean" the code generated from TouchGFX Designer directly, or can it only be done through the CUBE IDE?

6 replies

MM..1
Super User
July 28, 2021

Explain more Removed the button compiled and executed with stm32cubeide

Zu_it
Zu_itAuthor
Associate II
July 28, 2021

I removed the button with that background (image_Dark_Slider_Vertical_Medium_Slider3_Vertical_fill) from touchgfx by clicking on it and pressing CANC.

It works in simulation using touchgfx but then gives the error when I compile the project from stm32cubeide

Zu_it
Zu_itAuthor
Associate II
July 28, 2021

I updated Stm32Cube from 1.6.1 to 1.7.0 and this problem is solved, but do not know what is the cause.

AAdam.2
Visitor II
November 3, 2021

I'm running version 1.7 and the same thing happened. no clue how to fix it. I guess I'll just start fresh again. Touch gfx is cool, but there is a lot happening in the background, so when things break you are pretty much SOL.

Romain DIELEMAN
ST Employee
November 4, 2021

Hi,

​

The way I fix this is usually by opening the .project in notepad++ (or other code editor) and look for the lines related to that images that were removed and that cause issues. I then delete them. I am unsure if it is a STM32CubeIDE or a TouchGFX issue where this is not properly cleaned, I'll ask around again. I do't always face it but it is really annoying when I do I won't lie :grinning_face_with_sweat:.

​

/Romain

AAdam.2
AAdam.2Best answer
Visitor II
November 4, 2021

Hi Roman,

Thank you for the feedback. Well after I wrote that I figured.. HEY!!, I'm not going to let this thing beat me, and I better figure it out incase it happens again (which is a pretty safe bet probably). All I ended up having to do was go into application/user/generated/ and delete the .cpp files that were associated with the removed images from tGFX designer. They were obvious because then were marked with a '!'. The files were completed empty, but still in the file system.

Is there a way to "clean" the code generated from TouchGFX Designer directly, or can it only be done through the CUBE IDE?