Skip to main content
Angle
Associate III
Jan 15, 2023 11:00 AM UTC
Question

No rule to make target 'TouchGFX/build/STM32H750B-DK/Middlewares/Third_Party/FreeRTOS/Source/croutine.o', needed by 'TouchGFX/build/bin/target.elf'. Stop.

how can I solve this problem?

I already cleaned and rebuild the project but the error not missing

the error comes when I try to run the target on touchgfx bcs the error coming from touchgfx. stm32cubeIDE is okay and got no error.

0693W00000Y8FwWQAV.png 

This topic has been closed for replies.

13 replies

Romain DIELEMAN
ST Employee
Jan 16, 2023 4:34 AM UTC

Hi,

I do not have the board myself so I cannot test it but could you confirm that you are working with a project created from TouchGFX Designer with the TouchGFX Board Setup for the STM32h750dk ? What version of TouchGFX Designer are you using ?

/Romain

Angle
AngleAuthor
Associate III
Jan 16, 2023 5:49 AM UTC

yes , I working start from the scratch on Touchgfx . using version 4.21

Romain DIELEMAN
ST Employee
Jan 16, 2023 5:55 AM UTC

From scratch you mean starting from TouchGFX Designer right ? not from scratch from STM32CubeMX ? Sorry for the clarification question :grinning_face_with_sweat: