Skip to main content
MReus.2
Associate II
Sep 21, 2024 12:17 AM UTC
Solved

No reaction to detected touch custom H745I-Disco board

Hello,

i am working on a board that is redrawn from the H745I-Disco which originally has the FT5336 as touch controller. My Display has the FT5426. On an earlier board that recreated the F746-Disco (which also has the FT5336) i noticed that the  FT5426 worked right away. This was not the case on the H745 but was fixed after changing the Device ID. So touches are detected and deliver the proper values for x and y in sampleTouch() but nothing reacts to it. It is like there is no touch functionality at all. Any recommendations?

 

Thanks in advance!

Martin

This topic has been closed for replies.
MReus.2
MReus.2Best answer
Associate II
Sep 29, 2024 8:36 AM UTC

Hi Gaetan,

thank you very much for your reply. You summarized my problem correctly. The thing that didnt catch my eye right away was that x and y coordinates where swapped. As soon as i assigned x to y and y to x it started working. 

The difference between the FT53 and FT54 seems to be quite a bit more but since there is no multi touch in touch gfx it can be a cheap workaround i guess and it works from a user perspective. 

Thanks for your effort!!

3 replies

GaetanGodart
ST Employee
Sep 27, 2024 12:40 PM UTC

Hello @MReus.2 ,

 

To summarize:

  • previously you did a redraw of F746-DK to go from FT53 to FT54 and it worked straight away without changing anything
  • now you you did a redraw of F745-DK to go from FT53 to FT54 and you had to change the ID, now you get the right values in sampleTouch()

Are you sure that your GUI has clickable area?

Are you sure that your screen has touch?

Do you hand touch coordinates to the touchgfx framework,

Can you share your sampleTouch() function?

 

Regards,

Gaetan GodartSoftware engineer at ST (TouchGFX)
MReus.2
MReus.2AuthorBest answer
Associate II
Sep 29, 2024 8:36 AM UTC

Hi Gaetan,

thank you very much for your reply. You summarized my problem correctly. The thing that didnt catch my eye right away was that x and y coordinates where swapped. As soon as i assigned x to y and y to x it started working. 

The difference between the FT53 and FT54 seems to be quite a bit more but since there is no multi touch in touch gfx it can be a cheap workaround i guess and it works from a user perspective. 

Thanks for your effort!!

GaetanGodart
ST Employee
Sep 30, 2024 9:09 AM UTC

Hello @MReus.2 ,

 

I am glad you resolved your problem! :smiling_face_with_smiling_eyes:

 

Regards,

Gaetan GodartSoftware engineer at ST (TouchGFX)