Skip to main content
Visitor II
Apr 11, 2025 8:00 AM UTC
Question

Need to access a function in a customContainer triggered by selecting an item in a scrollist

Hi!

I have an issue with one of my implementations. 

 

void CalendarRepetitiveDaysView::scrollListProgramsUpdateItem(CustomContainerPrograms& item, int16_t itemIndex)

{

getWeekPrograms();

if (itemIndex < programCount)

{

WeekdayProgramGroup& program = weekdayPrograms[itemIndex];

TypedTextId type = getTypeOfProgram(program.active_favorite, program.standby_active);

item.updateTypeText(type);

item.updateTimeText(program.start_hour, program.start_min, program.hour_duration, program.min_duration);

item.updateWeekdayText(program.weekdays, program.weekday_or_not, program.day, program.month);

if (itemIndex == selectedIndex)

{

item.triggerProgramInfo(selectedProgram.start_hour,selectedProgram.start_min, selectedProgram.hour_duration, selectedProgram.min_duration,type, selectedProgram.temp, selectedProgram.hum);

customContainerProgramInfo1.setVisible(true);

customContainerProgramInfo1.invalidate();

}

}

}

 

void CalendarRepetitiveDaysView::scrollListPrograms_ItemSelectedHandler(int16_t itemSelected)

{

if (itemSelected < programCount)

{

selectedIndex = itemSelected;

selectedProgram = weekdayPrograms[itemSelected];

selectedProgramSet = true;

 

scrollListPrograms.invalidate();

 

}

}

 

This screen has one CustomContainerPrograms and one CustomContainerProgramInfo.

The CustomContainerPrograms holds the info for the scrollist, while the the CustomContainerProgramInfo

holds the info about each program. CustomContainerProgramInfo is a pop-up window that should

appear when selecting a program and contain the information about that program. The problem is that

I need to trigger a function in the CustomContainerProgramInfo to modify the info depending on what program it is.

So I tried instead to access it through CustomContainerPrograms to then call the function in CustomContainerProgramInfo.

But this approach will not work since it will not update as soon as I have a selected program.

Do you have any suggestions?

 

This topic has been closed for replies.