Skip to main content
Associate
Jan 6, 2025 9:10 AM UTC
Question

My touchgfx screen is glitched and project broke after touchgfx update (4.23.0 -> 4.24.2)

Hi,

 

I'm currently developping an application that need a tactile screen to run, i'm using the STM32F746G-Discovery board, and the project was in a finished state by June 2023. I re-used it now, and I saw that when flashing my old code into new board, the screen was all glitchy (a complete pixel non-sense of all color without any special logic). From the debugger, the program is crashed and called a Hardfault callback. The stack trace indicate clearly that it comes from the touchgfx part.

I tried then to create a blank touchgfx project in the version of my old project (4.23.0) and to flash it, the bug occur. And when I create a project from the 4.24.2 version (the last one then) it work as intended. So I concluded that this was just an update problem, but when I do the full touchgfx update procedure according to the guides, the problem still persist. I do the following :

- Open my old project in TouchGFX Designer 4.24.2 to update it, generate code through it
- Go to STM32Cube ioc file, migrate to the newer version of touchgfx through the component selector
- Generate code
- Compile and run

And then nothing changes, someone may get an idea on what am i doing wrong ?

I would like to precise that this exact problem happens to all my old projects (I have 3 touchgfx exemples of that), the only thing that changed is the st-link firmware forced upgrade I guess, since I didn't touched anything else. The whole thing seems realy weird to me. I also already tried to upgrade to the 4.24.0 first just in case.

 

Thanks to you all in advance for your help,

Best regards !

This topic has been closed for replies.

4 replies

GaetanGodart
ST Employee
Jan 7, 2025 1:31 PM UTC

Hello @Florian37 ,

 

I noticed that you mention using a new board. You also say that creating a new project from TouchGFX Designer 4.24.2 works fine.
Can you check which version is that board and which version was the previous one.
There was a major change in the board revision CU4 and later uses a new memory.

If that is your case, the simplest way to fix it is to create a new project and then clicking on "Edit" => "Import" => "GUI".

GaetanGodart_0-1736256605018.png

If you have a complex project where there is code outside of the TouchGFX scope, either you have to manually add it or I could maybe provide you with the git commit change that switch from the old memory to the new one.

 

Regards,

Gaetan GodartSoftware engineer at ST (TouchGFX)
Florian37Author
Associate
Jan 7, 2025 3:37 PM UTC

Hello @GaetanGodart , 

I really appreciate your help; you are absolutely right: old boards used CU2 revision, while the actual ones are on CU4. Sadly, the code is mostly external, so I would be glad to see this Git commit change. The GUI part never had bothered me, I used to copy the components directly from a .touchgfx file to another.

I saw a post with someone that has the exact same screen problem as mine where you already responded, here (https://community.st.com/t5/stm32-mcus-touchgfx-and-gui/stm32f746g-discovery-what-is-the-difference-between-cu3-and-cu4/td-p/744612) and it seems correlated. 

 

I can totally re-migrate projects for the new CU4 manually; I just hope I won't have to do it every time in the future.

 

Thanks for your reactiveness!

Best regards,

Florian

GaetanGodart
ST Employee
Jan 8, 2025 9:26 AM UTC

Hello @Florian37 ,

 

Perhaps the attached patch file would allow you to fix the issue without having to re-migrate everything.
To apply it do "git apply patchName.patch" (you need to use git I guess).

 

Regards,

Gaetan GodartSoftware engineer at ST (TouchGFX)