Skip to main content
Roman REITER
Associate III
Dec 29, 2022 3:46 PM UTC
Question

multiple events or multiple mixins in touchgfx

How can I use multiple events or multiple mixins in touchgfx. I've managed to use only one so far (like here). If I want to use several, I can't pass 2 callbacks to the view's constructor (in Screen1View.cpp).

Screen1View::Screen1View():boxMoveAnimationEndedCallback(this, &Screen1View::boxMoveAnimationEndedHandler), boxClickedCallback(this, &Screen1View::boxClickHandler) { }

When i select an event in touchgfx the following structure can be see

(in Screen1ViewBase.hpp).

touchgfx::MoveAnimator< touchgfx::Box > box1;

If I use several, the structure is different

touchgfx::ClickListener< touchgfx::MoveAnimator< touchgfx::Box > > box1;

Does somebody has any idea? is it even possible to use multiple mixins?

This topic has been closed for replies.

1 reply

Osman SOYKURT
ST Technical Moderator
Jan 2, 2023 9:57 AM UTC

Hello RReit.1,

Yes it's possible to use multiple mixins. Let's say you have a TextureMapper (that we call myTextureMapper) with both ClickListener and MoveAnimaor mixins.

In your hpp file file you need to have something like this:

 //Declaration of needed Handlers
 virtual void textureMapperAnimationEndedHandler(const AnimationTextureMapper& src);
 virtual void textureMapperClickHandler(const touchgfx::MoveAnimator< touchgfx::AnimationTextureMapper >& b, const ClickEvent& e);
 
 
 //Callback for Texture mapper : triggered when animation ends
 Callback<FactoryView, const AnimationTextureMapper&> textureMapperAnimationEndedCallback;
 
 //Callback for Texture mapper : triggered when clicked
 Callback<FactoryView, const touchgfx::MoveAnimator< touchgfx::AnimationTextureMapper > &, const ClickEvent&> textureMapperClickedCallback;

Then in your cpp , you'll pass it to the constructor like this :

Screen1View::Screen1View() :
 textureMapperAnimationEndedCallback(this, &FactoryView::textureMapperAnimationEndedHandler),
 textureMapperClickedCallback(this, &FactoryView::textureMapperClickHandler)
{ }

And then you'll associate the widget to the callback in the setupScreen() function for example :

void Screen1View::setupScreen()
{
 myTextureMapper.setTextureMapperAnimationEndedAction(textureMapperAnimationEndedCallback);
 myTextureMapper.setClickAction(textureMapperClickedCallback); 
}

Hope that helps.

/Osman

ST Software Developer | TouchGFX