Skip to main content
Sahil Ahmad
Associate
Oct 4, 2020 4:42 PM UTC
Question

multi touch controller ILI2511 USB interface

I am having 10.1 Inch display with CTP. The touch controller is ILI2511 at USB interface only. It is configured as multi touch point touch pad.

I connected touch panel with PC, it is detected by PC and multi touch test screen appears on PC screen, where I can see touch point where I touches the touch panel.

I want to use this panel with STM32H7 MCU at USB interface. Can anyone help.

This topic has been closed for replies.

2 replies

Alexandre RENOUX
Visitor II
Oct 5, 2020 4:43 AM UTC

Hello,

We do not have examples with USB interface touch controller.

However the principle is simple. In STM32TouchController.cpp file situated in TouchGFX/target/ folder, you initialize your touch controller driver (see void STM32TouchController::init()) and then in bool STM32TouchController::sampleTouch(int32_t& x, int32_t& y) you retrieve the coordinates from your TouchController. You can look at any Application Template available in TouchGFX Designer that has a touchable screen for reference. Note that you need to have a working driver in order to make things possible. Also TouchGFX do not support multi touch so you will only be able to pass one point coordinates at a time to the framework.

/Alexandre

Zakba.1
Associate III
Nov 18, 2023 1:10 PM UTC

hello 

could you finally drive it?I have the same problem and I need help