Skip to main content
Breeze1
Associate III
December 25, 2019
Question

More than one widget , how to refresh once together?

In Screen, I have 3 or more widgets , they are the same type of widget, but can not make them in one container. In normal , I have to invalid one by one. Now , I need them to refresh together, how do I do?

This topic has been closed for replies.

2 replies

HP_it
Senior II
December 25, 2019

the refresh rate is so high that invalidating them one by one should be fine?

another option could be to update the widgets when you enter the screen. use the activate method in the presenter to do that.

Breeze1
Breeze1Author
Associate III
December 26, 2019

For low power reason, we slow down the refresh rate. Now the refresh rate is no more than 10. If invalidating one by one , it will stuck.