Skip to main content
HGran.1
Associate II
November 22, 2020
Question

Migrating from TouchGFX 4.13 project to 4.15 prevents original user added imagery that was in (_designer) folder from being assignable to controls in 4.15 Designer

Good Morning,

I have a project created in TouchGFX 4.13 with user images that were automatically placed into a folder named _designer. Although 4.15 can display those images in the Images tab, they are not assignable to any newly added controls. They don't even show up in the image selection UI (The original controls image bindings still work, but can't assign them to newly added controls.

I found by renaming the _designer folder to Designer, and relaunching, the user image assets work fine again.

Am I correct to assume that TouchGFX 4.15 internally uses some unpublished folder name/prefix information to restrict UI visibility?

If so, is there a list of other hardcoded folder names, prefixes that have non-standard functionality in TouchGFX 4.15?

Thanks,

Heather

This topic has been closed for replies.

2 replies

Bob Bailey
Senior
November 24, 2020

is there a guide to migrating? I am getting ready to do this (4.13 to 4.15)

Thanks,

Bob Bailey

Alexandre RENOUX
Visitor II
November 27, 2020

Hello,

I personally migrated a UI from 4.13 to 4.15 and everything was fine.

Can you try deleting the _designer before trying the migration ?

If it does not resolve the problem, could you elaborate ? Because I'm not sure I follow your point otherwise.

/Alexandre