Skip to main content
Associate II
Aug 26, 2024 12:13 AM UTC
Question

memory limit question

There was an issue where the screen froze due to too many packages. Is there a way in TouchGFX to check the memory limit for a screen and the amount of memory each package uses to evaluate the number of packages that can be used?

    This topic has been closed for replies.

    3 replies

    ST Employee
    Aug 28, 2024 11:31 AM UTC

    Hello @yu_jay ,

    I dont fully understand the question, what do you mean by "package" ? And you are running on target or in the simulator ?

    Best regards,

    Louis B.

    Louis BOUDOST Software Engineer | TouchGFX
    yu_jayAuthor
    Associate II
    Oct 28, 2024 3:46 AM UTC

     

     

    1. In this context, does "package" mean how many toolkits are used in a single screen before causing errors?
    2. Under what conditions could the attached error occur?

     

     

    ST Employee
    Nov 19, 2024 2:32 PM UTC

    Hello @yu_jay ,

    I dont understand what you mean by package/toolkits, are you talking about the widgets (TextArea, Box etc ?), if so the "memory limit" depends on the setup you have. You have to calculate the objects you have and see if you have enough RAM available.

    The message you have is too generic it can be a lot of things.

    Best regards,

    Louis BOUDOST Software Engineer | TouchGFX