Skip to main content
Senior
Mar 11, 2025 2:51 AM UTC
Solved

"LTDC" option not available as Application Tick Source in X-CUBE-TOUCHGFX

Hi,

as you can see in the first screenshot, in the X-CUBE-TOUCHGFX settings (TouchGFX Generator tab) the LTDC option for the Application Tick Source is not available. And at the bottom it says "LTDC in only available if enabled".

LTDC is enabled and configured (second screenshot). Does it need to be configured and/or enabled in some other ways or some other place too?

Thank you :)

 

Ricko_0-1741661353205.png

Ricko_1-1741661458299.png

 

 

This topic has been closed for replies.
jchernus-fikst
jchernus-fikstBest answer
Senior
Mar 11, 2025 10:37 AM UTC

Yes, in your first screenshot, under Display -> Interface, you have the change the value from Custom to LTDC.

5 replies

jchernus-fikst
jchernus-fikstBest answer
Senior
Mar 11, 2025 10:37 AM UTC

Yes, in your first screenshot, under Display -> Interface, you have the change the value from Custom to LTDC.

RickoAuthor
Senior
Mar 11, 2025 3:29 PM UTC

Thank you @jchernus-fikst

but as you can see it is greyed out and cannot be selected. I was asking why and what else I would need to enable in order for it to not be greyed out so I can select it.

Thank you :)

jchernus-fikst
Senior
Mar 12, 2025 10:21 AM UTC

Please re-read my answer.

Your question asked about Driver -> Application Tick Source. I'm suggesting you change Display -> Interface. These are two different things. 

Julia

RickoAuthor
Senior
Mar 12, 2025 4:21 PM UTC

Sorry @jchernus-fikst long days i front of the PC, I misread your answer.

Yes, now it works.

Thank you! :)