Skip to main content
Associate
Sep 16, 2025 12:22 AM UTC
Question

LTDC configuration problem with STM32L4R9 and 2.1" NewHaven round display.

Hello everyone,

I’m working on a custom board based on the STM32L4R9 with a 2.1" round 480×480 display from Newhaven, which uses the ST7701S controller. My goal is to get it running with MIPI DSI / LTDC and TouchGFX.

So far, I’ve managed to display a solid color by manually filling a framebuffer. However, once I integrated TouchGFX and started rendering shapes, the lines appeared shifted. This makes me think the issue is related to timing parameters (HSYNC, VSYNC, VBP, VFP, HBP, HFP).

The problem is that the display datasheet doesn’t provide typical timing values. I contacted Newhaven’s support, and they shared example code for the same panel but using the SSD1963 controller. Unfortunately, using those values didn’t work. Looking deeper into their example, I noticed that the comments mention one set of values, but the actual register settings differ. When I reached out again, they simply said the comments might be wrong, but the code should work. Not very helpful.
Here is the example that they have provided and as you can clearly see: 

command(0xb4); //SET HBP
 data(0x03); //SET HSYNC Total=1056
 data(0xA0);
 data(0x00); //SET HBP 88
 data(0x58);
 data(0x80); //SET HSYNC Pulse Width=128=127pixels+1
 data(0x00); //SET Hsync pulse start position
 data(0x00);
 data(0x00); //SET Hsync pulse subpixel start position
 command(0xb6); //SET VBP
 data(0x02); //SET Vsync total 525
 data(0x0d);
 data(0x00); //SET VBP=32
 data(0x1F);
 data(0x01); //SET VSYNC Pulse Width= 0=0lines+1
 data(0x00); //SET Vsync pulse start position
 data(0x00);

HSYNC total value in the comment is 1056 but the real value is 0x03A0 which is 928, that made me doubt all the values.

Has anyone here worked with this display before? If so, could you share the correct timing parameters?
I’ll attach both the expected output and the actual result I’m getting.

Thanks in advance!

5 replies

Associate II
Nov 5, 2025 2:00 AM UTC

Hi Seyli, how are you? I've read your post and I thinking of developing a product with the same combination as yours (STM32L4R9I + 2.1" NewHaven round display). Were you able to make it work?

 

Thanks!

SeyliAuthor
Associate
Nov 5, 2025 2:18 AM UTC

Hi, yes after a lot of debugging I was able to make it work :D let me know if you need help 

Associate II
Nov 5, 2025 2:33 PM UTC

It’s great to hear that, Seyli, and thank you for getting back to me so quickly. It’s good to know that controlling the LCD with the STM32L4R9 is feasible.

At the moment I don’t have my own hardware designed to drive the display, so as a proof of concept I’m planning to use the STM32L4R9I-DISCO development kit and replace the display board (MB1314C-01) with my own, which would allow me to connect the MIPI‑DSI signals to the NewHaven LCD.

The wiring would be as shown in the attached image (MB1314‑to‑NewHaven‑2‑inches‑display.png). I understand that, since the LCD would be driven through its MIPI‑DSI interface in video mode, the RGB and SPI pins on the LCD would not be used.

Regarding the software, I wanted to ask: given that the display is 480×480, it isn’t possible to use the microcontroller’s internal memory to store the frame buffer, so in your PCB design did you use an external PSRAM?

Also, because the LCD has the internal SS7701 controller, it needs a driver to control it via MIPI‑DSI and the MCU’s LTDC peripheral has to be configured correctly. I’ve been looking at the driver provided by user JMD in the following link (they say it works for a square display with the SS7701):

https://community.st.com/t5/stm32-mcus-touchgfx-and-gui/is-stm32f769iit-feasible-with-st7701-and-nt35510mh-lcd-ic-driver/td-p/190562/page/3

When you developed your solution, did you use that project as a starting point?

Any suggestions or comments about issues you encountered would be very helpful to me.

Many thanks again.