Lots of errors when building basic project
- 7 replies
- 2672 views
I have a CubeIDE project for a H743IITx board and an LCD and I added Touchgfx. The Touchgfx 4.24 contains the typical demo that switches between two screens. It runs fine in the simulator. I refreshed the project and it added all the necessary folders/files. Touchgfx is installed on the PC and the package was added inside the CubeIDE manager.
As you can see in the screenshot, there are a lot of red underlined files when I attempt to build the project. There are about 240 errors.
Usually, when so much code is underlined, it's a matter of missing libraries due to some kind of incomplete setup. However, I don't know what is wrong. I followed the documentation setup as well as different videos on youtube and actually the initial setup is not that complex.
Any ideas what could be missing?