Long rendering time when moving two images
Hi @Martin KJELDSEN
On a screen I want to move two large images (one has transparency). I've implemented it like in your birdgame example (with the moveto(x,y) method.
Now I recognized that the animation is very slow and the rendering time is very long (>30ms). I don't know why this take so long. I measured it with the RENDER_TIME GPIO and also in SW. I see that the TouchGFX Library is active for more than 30ms.
Do you have any idea where the issue come from? Below you will find the implementation
Thank you
Best regards
Marco
#include <gui/containers/container_moving_waves.hpp>
#include <BitmapDatabase.hpp>
#include <touchgfx/Color.hpp>
container_moving_waves::container_moving_waves(): m_waveForeground(),
m_waveBackground(),
m_animationState(AnimationState::AnimationRunning),
m_tickCounter(0U),
m_tickinterval(1U) {}
void container_moving_waves::initialize()
{
container_moving_wavesBase::initialize();
initializeLayer(m_waveBackground, BITMAP_WAVE_BACKGROUND_ID, 255U, 1U, -1);
initializeLayer(m_waveForeground, BITMAP_WAVE_FOREGROUND_ID, 204U, 1U, 1);
m_boxWave.setPosition(0, 217, 800, 33);
m_boxWave.setColor(touchgfx::Color::getColorFrom24BitRGB(112, 148, 197));
add(m_boxWave);
}
void container_moving_waves::startAnimation() {
m_animationState = AnimationState::AnimationRunning;
}
void container_moving_waves::stopAnimation() {
m_animationState = AnimationState::NoAnimation;
}
void container_moving_waves::handleTickEvent() {
m_tickCounter++;
if ((m_tickCounter % m_tickinterval) != 0U) {
return;
}
if (m_animationState == AnimationState::AnimationRunning) {
moveLayer(m_waveForeground, m_tickCounter);
moveLayer(m_waveBackground, m_tickCounter);
}
}
void container_moving_waves::initializeLayer(Layer& layer, const BitmapId bmp, uint8_t alpha, const uint32_t animationUpdateSpeed, const int32_t animationWidth)
{
layer.image0.setBitmap(Bitmap(bmp));
layer.image1.setBitmap(Bitmap(bmp));
layer.image0.setXY(0, 0U);
if (animationWidth < 0) {
layer.image1.setXY(layer.image0.getRect().right(), 0U);
}
else {
layer.image1.setXY(layer.image0.getRect().x - layer.image1.getWidth(), 0U);
}
layer.image0.setAlpha(alpha);
layer.image1.setAlpha(alpha);
add(layer.image0);
add(layer.image1);
layer.animationUpdateSpeed = animationUpdateSpeed;
layer.animationWidth = animationWidth;
}
void container_moving_waves::moveLayer(Layer& layer, const uint32_t tickCount) {
if ((tickCount % layer.animationUpdateSpeed) == 0U) {
layer.image0.moveTo(layer.image0.getX() + layer.animationWidth, layer.image0.getY());
layer.image1.moveTo(layer.image1.getX() + layer.animationWidth, layer.image1.getY());
if (layer.animationWidth < 0) {
//when moving left
if (layer.image0.getRect().right() < 0) {
layer.image0.moveTo(layer.image1.getRect().right(), layer.image0.getY());
}
if (layer.image1.getRect().right() < 0) {
layer.image1.moveTo(layer.image0.getRect().right(), layer.image1.getY());
}
}
else {
//when moving right
if (layer.image0.getRect().x > layer.image0.getWidth()) {
layer.image0.moveTo(layer.image1.getRect().x - layer.image0.getWidth(), layer.image0.getY());
}
if (layer.image1.getRect().x > layer.image1.getWidth()) {
layer.image1.moveTo(layer.image0.getRect().x - layer.image1.getWidth(), layer.image1.getY());
}
}
}
}