Skip to main content
RReta.1
Associate II
January 21, 2021
Solved

Links to TouchGFX Documentation: Backend Communication examples not working

Hello,

I want to download sample code from this page: https://support.touchgfx.com/docs/development/ui-development/touchgfx-engine-features/backend-communication

But I don't think the links are working, for example:

http://sw-center.st.com/touchgfx/TouchGFX/knowledgebase/hw_integration_tasks_exti.4.9.3.zip

Does not download the zip. I think the links maybe broken again.

Is there an updated link we can use to get the example code?

Thanks!

This topic has been closed for replies.
RReta.1
RReta.1Best answer
Associate II
January 22, 2021

Hi Romain,

Thanks for the response and hint! I was able to download from another browser.

The browser I was using was Chrome version 87.0.4280.141 (Official Build) (x86_64).

When it was not working, none of the .zip download links on the page seems to work.

/RR

3 replies

Romain DIELEMAN
ST Employee
January 22, 2021

Hi,

This is very odd as I am able to download it on my side. What browser are you using ? Do the other links work or is it only that one in your case ?

/Romain

RReta.1
RReta.1AuthorBest answer
Associate II
January 22, 2021

Hi Romain,

Thanks for the response and hint! I was able to download from another browser.

The browser I was using was Chrome version 87.0.4280.141 (Official Build) (x86_64).

When it was not working, none of the .zip download links on the page seems to work.

/RR

Romain DIELEMAN
ST Employee
January 25, 2021

Good to hear that you were able to download the zip you needed. I'll try to see if I can replicate that issue with the same Chrome version when I can just to check :ok_hand:.

/Romain