Skip to main content
Associate III
May 15, 2025 3:39 PM UTC
Question

Linker errors for sensor data processing functions in STM32CubeIDE + TouchGFX

Hello everyone,

I’m developing an STM32H750 application using STM32CubeIDE and TouchGFX, and I’m trying to integrate a sensor using I2C.

I implemented a sensor driver and added the corresponding source files, but I’m running into linker errors like:

undefined reference to `Sensor_Calc()'

I made sure the source files are included in the build and headers properly referenced, but the errors persist.

If anyone has working examples, suggestions, I’d be grateful.

Thanks for your help!

Additional Info:

  • STM32CubeIDE version: 1.17.0

  • Compiler: arm-none-eabi-gcc 12.3.1

  • Target MCU: STM32H750B-DK

  • Using C++ and TouchGFX framework

This topic has been closed for replies.

7 replies

Nathan_Xi
Associate III
May 16, 2025 1:57 AM UTC

Hello @Rafla 

Maybe you can present more details.

It's hard to identify your bug with the information given.

Thanks.

RaflaAuthor
Associate III
May 17, 2025 10:39 PM UTC

The code compiles fine on the real target, but when I try to build the TouchGFX Simulator, I get the following error repeatedly:

fatal error: i2c_data.h: No such file or directory

The i2c_data.h file is present in my project under Core/Inc.

It seems the simulator build does not include the folder containing i2c_data.h in its include paths.

MM..1
Super User
May 16, 2025 5:14 AM UTC

You dont show code , but for C++ you maybe skip use right C headers...

Learn how use 

#ifdef __cplusplus
 extern "C" {
#endif
RaflaAuthor
Associate III
May 17, 2025 10:35 PM UTC

The code compiles fine on the real target, but when I try to build the TouchGFX Simulator, I get the following error repeatedly:

fatal error: i2c_data.h: No such file or directory

The i2c_data.h file is present in my project under Core/Inc.

It seems the simulator build does not include the folder containing i2c_data.h in its include paths.