Skip to main content
Kostas Papouis
Associate III
Oct 22, 2024 10:11 PM UTC
Solved

Link Hardware button with "Button With Label"

Hello Community,

I have few "Buttons with Labels" within a scroll list where I am able to scroll within the scroll list using a hardware button and animateToItem function.

What I would also like to do is to show which Button with label is active.

Is there any way a hardware button can be linked with a Button with Label.
Thank you in advance.

 

 

This topic has been closed for replies.
ST Employee
Oct 23, 2024 2:50 PM UTC

Hello @Kostas Papouis,

You can use Scroll Wheel instead of Scroll List which already supports a functionality to highlight the selected button. You just need to provide the image for when the button is selected. 
There are a lot of examples available in the TouchGFX Designer that you can use for inspiration. For instance, you can take a look at TouchGFX Demo 5 in the language selection screen. 

TouchGFX Demo 5TouchGFX Demo 5 

For your second question, there is no direct way to connect a hardware button to ButtonWithLabel; however, you can simply define an Interaction to happen when a specific hardware button is pressed. There is also example for that in TouchGFX Demo 5.

I hope this helps you!
Don't hesitate to ask more questions if you have any!

Mohammad MORADIST Software Developer | TouchGFX

2 replies

ST Employee
Oct 23, 2024 2:50 PM UTC

Hello @Kostas Papouis,

You can use Scroll Wheel instead of Scroll List which already supports a functionality to highlight the selected button. You just need to provide the image for when the button is selected. 
There are a lot of examples available in the TouchGFX Designer that you can use for inspiration. For instance, you can take a look at TouchGFX Demo 5 in the language selection screen. 

TouchGFX Demo 5TouchGFX Demo 5 

For your second question, there is no direct way to connect a hardware button to ButtonWithLabel; however, you can simply define an Interaction to happen when a specific hardware button is pressed. There is also example for that in TouchGFX Demo 5.

I hope this helps you!
Don't hesitate to ask more questions if you have any!

Mohammad MORADIST Software Developer | TouchGFX
Kostas Papouis
Associate III
Oct 26, 2024 4:10 PM UTC

Thank you.