Skip to main content
STran.2
Associate II
November 20, 2020
Question

libtouchgfx-float-abi-hard.a cause build error in STM32CubeIDE

I followed instrunction in this online workshop STM32 Graphics Workshop - 10 TouchGFX lab temperature sensor display https://www.youtube.com/watch?v=rYrRjXyAYvs&list=PLnMKNibPkDnGNY9Ny4FWpM5bgC3b4XdbN&index=10

When I get to (minute 18:30) the step build in STM32CubeIDE I get this error list below. Please help.

17:31:33 **** Incremental Build of configuration Debug for project STM32H7B3I_DISCO ****

make -j4 all 

arm-none-eabi-g++ -o "STM32H7B3I_DISCO.elf" @"objects.list" -l:libtouchgfx-float-abi-hard.a -mcpu=cortex-m7 -T"C:\TouchGFXProjects\STM32H7BWorkshop2020\STM32CubeIDE\STM32H7B3LIHXQ_FLASH.ld" --specs=nosys.specs -Wl,-Map="STM32H7B3I_DISCO.map" -Wl,--gc-sections -static -L"C:\TouchGFXProjects\STM32H7BWorkshop2020\STM32CubeIDE\Middlewares\ST\touchgfx\lib\core\cortex_m7\gcc" -L"C:/_SandBox/2020_WShp_GFX/Lab/STM32H7BWorkshop2020_NSA/Middlewares/ST/touchgfx/lib/core/cortex_m7/gcc" -L"C:/STM32H7BWorkshop2020/DryRun/STM32H7BWorkshop2020/Middlewares/ST/touchgfx/lib/core/cortex_m7/gcc" -L"C:/_Temp/STM32H7BWorkshop2020/STM32H7BWorkshop2020/Middlewares/ST/touchgfx/lib/core/cortex_m7/gcc" -L"C:/STM32H7BWorkshop2020/STM32H7BWorkshop2020/Middlewares/ST/touchgfx/lib/core/cortex_m7/gcc" -L"C:/2020_ST_GFX_WS/STM32H7BWorkshop2020/Middlewares/ST/touchgfx/lib/core/cortex_m7/gcc" -LC:/TouchGFXProjects/STM32H7BWorkshop2020/Middlewares/ST/touchgfx/lib/core/cortex_m7/gcc --specs=nano.specs -mfpu=fpv5-d16 -mfloat-abi=hard -mthumb -Wl,--start-group -lc -lm -lstdc++ -lsupc++ -Wl,--end-group

C:\TouchGFXProjects\STM32H7BWorkshop2020\STM32CubeIDE\Middlewares\ST\touchgfx\lib\core\cortex_m7\gcc\libtouchgfx-float-abi-hard.a(LCD.o): In function `touchgfx::LCD::drawString(touchgfx::Rect, touchgfx::Rect const&, touchgfx::LCD::StringVisuals const&, unsigned short const*, ...)':

(.text._ZN8touchgfx3LCD10drawStringENS_4RectERKS1_RKNS0_13StringVisualsEPKtz+0x0): multiple definition of `touchgfx::LCD::drawString(touchgfx::Rect, touchgfx::Rect const&, touchgfx::LCD::StringVisuals const&, unsigned short const*, ...)'

Application/User/generated/Texts.o:C:/TouchGFXProjects/STM32H7BWorkshop2020/TouchGFX/generated/texts/src/Texts.cpp:51: first defined here

C:\TouchGFXProjects\STM32H7BWorkshop2020\STM32CubeIDE\Middlewares\ST\touchgfx\lib\core\cortex_m7\gcc\libtouchgfx-float-abi-hard.a(Font.o): In function `touchgfx::Font::getStringWidth(unsigned short const*, ...) const':

(.text._ZNK8touchgfx4Font14getStringWidthEPKtz+0x0): multiple definition of `touchgfx::Font::getStringWidth(unsigned short const*, ...) const'

Application/User/generated/Texts.o:C:/TouchGFXProjects/STM32H7BWorkshop2020/TouchGFX/generated/texts/src/Texts.cpp:14: first defined here

C:\TouchGFXProjects\STM32H7BWorkshop2020\STM32CubeIDE\Middlewares\ST\touchgfx\lib\core\cortex_m7\gcc\libtouchgfx-float-abi-hard.a(Font.o): In function `touchgfx::Font::getStringWidth(unsigned char, unsigned short const*, ...) const':

(.text._ZNK8touchgfx4Font14getStringWidthEhPKtz+0x0): multiple definition of `touchgfx::Font::getStringWidth(unsigned char, unsigned short const*, ...) const'

Application/User/generated/Texts.o:C:/TouchGFXProjects/STM32H7BWorkshop2020/TouchGFX/generated/texts/src/Texts.cpp:23: first defined here

C:\TouchGFXProjects\STM32H7BWorkshop2020\STM32CubeIDE\Middlewares\ST\touchgfx\lib\core\cortex_m7\gcc\libtouchgfx-float-abi-hard.a(Font.o):(.rodata._ZTVN8touchgfx4FontE+0x0): multiple definition of `vtable for touchgfx::Font'

Application/User/generated/Texts.o:(.rodata._ZTVN8touchgfx4FontE+0x0): first defined here

C:\TouchGFXProjects\STM32H7BWorkshop2020\STM32CubeIDE\Middlewares\ST\touchgfx\lib\core\cortex_m7\gcc\libtouchgfx-float-abi-hard.a(TextProvider.o): In function `touchgfx::TextProvider::initializeInternal()':

(.text._ZN8touchgfx12TextProvider18initializeInternalEv+0x0): multiple definition of `touchgfx::TextProvider::initializeInternal()'

Application/User/generated/Texts.o:C:/TouchGFXProjects/STM32H7BWorkshop2020/TouchGFX/generated/texts/src/Texts.cpp:46: first defined here

C:\TouchGFXProjects\STM32H7BWorkshop2020\STM32CubeIDE\Middlewares\ST\touchgfx\lib\core\cortex_m7\gcc\libtouchgfx-float-abi-hard.a(TextProvider.o): In function `touchgfx::TextProvider::getNextLigature(unsigned char)':

(.text._ZN8touchgfx12TextProvider15getNextLigatureEh+0x0): multiple definition of `touchgfx::TextProvider::getNextLigature(unsigned char)'

Application/User/generated/Texts.o:C:/TouchGFXProjects/STM32H7BWorkshop2020/TouchGFX/generated/texts/src/Texts.cpp:32: first defined here

Application/User/TouchGFX/target/generated/TouchGFXConfiguration.o:(.rodata._ZTV19FrontendApplication[_ZTV19FrontendApplication]+0x30): undefined reference to `touchgfx::Application::requestRedraw()'

Application/User/TouchGFX/target/generated/TouchGFXConfiguration.o:(.rodata._ZTV23FrontendApplicationBase[_ZTV23FrontendApplicationBase]+0x30): undefined reference to `touchgfx::Application::requestRedraw()'

Application/User/TouchGFX/target/generated/TouchGFXConfiguration.o:(.rodata._ZTVN8touchgfx14MVPApplicationE[_ZTVN8touchgfx14MVPApplicationE]+0x30): undefined reference to `touchgfx::Application::requestRedraw()'

collect2.exe: error: ld returned 1 exit status

make: *** [makefile:77: STM32H7B3I_DISCO.elf] Error 1

"make -j4 all" terminated with exit code 2. Build might be incomplete.

17:31:35 Build Failed. 6 errors, 0 warnings. (took 2s.49ms)

This topic has been closed for replies.

10 replies

Romain DIELEMAN
ST Employee
November 20, 2020

Hi,

I wont lie that it is a bit complicated to read that text :grinning_face_with_sweat:. Could you maybe share your project or add a screenshot of this error message ? (the colors will help us see faster where the issues are).

I have not gone through that video but I suppose you followed all the steps ?

/Romain

STran.2
STran.2Author
Associate II
November 24, 2020

The online training its starter files are based on TouchGFX 4.13. The generated Texts.cpp has a different format and methods from what the TouchGFX 4.14 generate. I uninstalled the version 4.14 and installed the version 4.13 and the labs work as expected. Enclosed are the 2 Texts.cpp files generated. You find this file under C:\TouchGFXProjects\STM32H7BWorkshop_lab4\TouchGFX\generated\texts\src

The errors caused by the four extra methods generated by the GFX Version 4.14

STran.2
STran.2Author
Associate II
November 24, 2020

Text.cpp from GFX Version 4.13

/* DO NOT EDIT THIS FILE */

/* This file is autogenerated by the text-database code generator */

#include <stdarg.h>

#include <touchgfx/Texts.hpp>

#include <touchgfx/hal/HAL.hpp>

#include <touchgfx/TypedText.hpp>

#include <texts/TypedTextDatabase.hpp>

#include <touchgfx/lcd/LCD.hpp>

#include <touchgfx/TextProvider.hpp>

touchgfx::Font::StringWidthFunctionPointer touchgfx::Font::getStringWidthFunction = &touchgfx::Font::getStringWidthLTR;

touchgfx::LCD::DrawStringFunctionPointer touchgfx::LCD::drawStringFunction = &touchgfx::LCD::drawStringLTR;

touchgfx::TextProvider::UnicodeConverterInitFunctionPointer touchgfx::TextProvider::unicodeConverterInitFunction = static_cast<touchgfx::TextProvider::UnicodeConverterInitFunctionPointer>(0);

touchgfx::TextProvider::UnicodeConverterFunctionPointer touchgfx::TextProvider::unicodeConverterFunction = static_cast<touchgfx::TextProvider::UnicodeConverterFunctionPointer>(0);

//Default typed text database

extern const touchgfx::TypedText::TypedTextData* const typedTextDatabaseArray[];

TEXT_LOCATION_FLASH_PRAGMA

KEEP extern const touchgfx::Unicode::UnicodeChar texts_all_languages[] TEXT_LOCATION_FLASH_ATTRIBUTE =

{

  0x4a, 0x75, 0x6e, 0x63, 0x74, 0x69, 0x6f, 0x6e, 0x20, 0x54, 0x65, 0x6d, 0x70, 0x65, 0x72, 0x61, 0x74, 0x75, 0x72, 0x65, 0x0, // @0 "Junction Temperature"

  0x54, 0x6f, 0x67, 0x67, 0x6c, 0x65, 0x20, 0x50, 0x68, 0x79, 0x73, 0x69, 0x63, 0x61, 0x6c, 0x20, 0x4c, 0x45, 0x44, 0x0, // @21 "Toggle Physical LED"

  0x54, 0x6f, 0x67, 0x67, 0x6c, 0x65, 0x20, 0x4c, 0x6f, 0x67, 0x69, 0x63, 0x61, 0x6c, 0x20, 0x4c, 0x45, 0x44, 0x0, // @41 "Toggle Logical LED"

  0x50, 0x72, 0x65, 0x76, 0x69, 0x6f, 0x75, 0x73, 0xa, 0x0, // @60 "Previous?"

  0x4e, 0x65, 0x78, 0x74, 0x0, // @70 "Next"

  0x53, 0x57, 0x0, // @75 "SW"

  0x48, 0x57, 0x0 // @78 "HW"

};

extern uint32_t const indicesGb[];

//array holding dynamically installed languages

struct TranslationHeader

{

  uint32_t offset_to_texts;

  uint32_t offset_to_indices;

  uint32_t offset_to_typedtext;

};

static const TranslationHeader* languagesArray[1] = { 0 };

//Compiled and linked in languages

static const uint32_t* const staticLanguageIndices[] =

{

  indicesGb

};

touchgfx::LanguageId touchgfx::Texts::currentLanguage = static_cast<touchgfx::LanguageId>(0);

static const touchgfx::Unicode::UnicodeChar* currentLanguagePtr = 0;

static const uint32_t* currentLanguageIndices = 0;

void touchgfx::Texts::setLanguage(touchgfx::LanguageId id)

{

  const touchgfx::TypedText::TypedTextData* currentLanguageTypedText = 0;

  if (id < 1)

  {

    if (languagesArray[id] != 0)

    {

      //dynamic translation is added

      const TranslationHeader* translation = languagesArray[id];

      currentLanguagePtr = (const touchgfx::Unicode::UnicodeChar*)(((const uint8_t*)translation) + translation->offset_to_texts);

      currentLanguageIndices = (const uint32_t*)(((const uint8_t*)translation) + translation->offset_to_indices);

      currentLanguageTypedText = (const touchgfx::TypedText::TypedTextData*)(((const uint8_t*)translation) + translation->offset_to_typedtext);

    }

    else

    {

      //compiled and linked in languages

      currentLanguagePtr = texts_all_languages;

      currentLanguageIndices = staticLanguageIndices[id];

      currentLanguageTypedText = typedTextDatabaseArray[id];

    }

  }

  if (currentLanguageTypedText)

  {

    currentLanguage = id;

    touchgfx::TypedText::registerTypedTextDatabase(currentLanguageTypedText,

                            TypedTextDatabase::getFonts(), TypedTextDatabase::getInstanceSize());

  }

}

void touchgfx::Texts::setTranslation(touchgfx::LanguageId id, const void* translation)

{

  languagesArray[id] = (const TranslationHeader*)translation;

}

const touchgfx::Unicode::UnicodeChar* touchgfx::Texts::getText(TypedTextId id) const

{

  return &currentLanguagePtr[currentLanguageIndices[id]];

}

STran.2
STran.2Author
Associate II
November 24, 2020

Text.cpp from GFX Version 4.14

/* DO NOT EDIT THIS FILE */

/* This file is autogenerated by the text-database code generator */

#include <stdarg.h>

#include <texts/TypedTextDatabase.hpp>

#include <touchgfx/TextProvider.hpp>

#include <touchgfx/Texts.hpp>

#include <touchgfx/TypedText.hpp>

#include <touchgfx/Unicode.hpp>

#include <touchgfx/hal/HAL.hpp>

#include <touchgfx/lcd/LCD.hpp>

uint16_t touchgfx::Font::getStringWidth(const touchgfx::Unicode::UnicodeChar* text, ...) const

{

  va_list pArg;

  va_start(pArg, text);

  uint16_t width = getStringWidthLTR(TEXT_DIRECTION_LTR, text, pArg);

  va_end(pArg);

  return width;

}

uint16_t touchgfx::Font::getStringWidth(touchgfx::TextDirection textDirection, const touchgfx::Unicode::UnicodeChar* text, ...) const

{

  va_list pArg;

  va_start(pArg, text);

  uint16_t width = getStringWidthLTR(textDirection, text, pArg);

  va_end(pArg);

  return width;

}

touchgfx::Unicode::UnicodeChar touchgfx::TextProvider::getNextLigature(TextDirection direction)

{

  if (fontGsubTable && nextCharacters.peekChar())

  {

    substituteGlyphs();

    if (nextCharacters.peekChar(1) == 0x093F) //Hindi I-matra

    {

      nextCharacters.replaceAt1(nextCharacters.peekChar());

      nextCharacters.replaceAt0(0x093F);

    }

  }

  return getNextChar();

}

void touchgfx::TextProvider::initializeInternal()

{

  fillInputBuffer();

}

void touchgfx::LCD::drawString(touchgfx::Rect widgetArea, const touchgfx::Rect& invalidatedArea, const touchgfx::LCD::StringVisuals& stringVisuals, const touchgfx::Unicode::UnicodeChar* format, ...)

{

  va_list pArg;

  va_start(pArg, format);

  drawStringLTR(widgetArea, invalidatedArea, stringVisuals, format, pArg);

  va_end(pArg);

}

//Default typed text database

extern const touchgfx::TypedText::TypedTextData* const typedTextDatabaseArray[];

TEXT_LOCATION_FLASH_PRAGMA

KEEP extern const touchgfx::Unicode::UnicodeChar texts_all_languages[] TEXT_LOCATION_FLASH_ATTRIBUTE =

{

  0x4a, 0x75, 0x6e, 0x63, 0x74, 0x69, 0x6f, 0x6e, 0x20, 0x54, 0x65, 0x6d, 0x70, 0x65, 0x72, 0x61, 0x74, 0x75, 0x72, 0x65, 0x0, // @0 "Junction Temperature"

  0x54, 0x6f, 0x67, 0x67, 0x6c, 0x65, 0x20, 0x50, 0x68, 0x79, 0x73, 0x69, 0x63, 0x61, 0x6c, 0x20, 0x4c, 0x45, 0x44, 0x0, // @21 "Toggle Physical LED"

  0x54, 0x6f, 0x67, 0x67, 0x6c, 0x65, 0x20, 0x4c, 0x6f, 0x67, 0x69, 0x63, 0x61, 0x6c, 0x20, 0x4c, 0x45, 0x44, 0x0, // @41 "Toggle Logical LED"

  0x50, 0x72, 0x65, 0x76, 0x69, 0x6f, 0x75, 0x73, 0xa, 0x0, // @60 "Previous?"

  0x4e, 0x65, 0x78, 0x74, 0x0, // @70 "Next"

  0x53, 0x57, 0x0, // @75 "SW"

  0x48, 0x57, 0x0 // @78 "HW"

};

TEXT_LOCATION_FLASH_PRAGMA

KEEP extern uint32_t const indicesGb[] TEXT_LOCATION_FLASH_ATTRIBUTE;

//array holding dynamically installed languages

struct TranslationHeader

{

  uint32_t offset_to_texts;

  uint32_t offset_to_indices;

  uint32_t offset_to_typedtext;

};

static const TranslationHeader* languagesArray[1] = { 0 };

//Compiled and linked in languages

static const uint32_t* const staticLanguageIndices[] =

{

  indicesGb

};

touchgfx::LanguageId touchgfx::Texts::currentLanguage = static_cast<touchgfx::LanguageId>(0);

static const touchgfx::Unicode::UnicodeChar* currentLanguagePtr = 0;

static const uint32_t* currentLanguageIndices = 0;

void touchgfx::Texts::setLanguage(touchgfx::LanguageId id)

{

  const touchgfx::TypedText::TypedTextData* currentLanguageTypedText = 0;

  if (id < 1)

  {

    if (languagesArray[id] != 0)

    {

      //dynamic translation is added

      const TranslationHeader* translation = languagesArray[id];

      currentLanguagePtr = (const touchgfx::Unicode::UnicodeChar*)(((const uint8_t*)translation) + translation->offset_to_texts);

      currentLanguageIndices = (const uint32_t*)(((const uint8_t*)translation) + translation->offset_to_indices);

      currentLanguageTypedText = (const touchgfx::TypedText::TypedTextData*)(((const uint8_t*)translation) + translation->offset_to_typedtext);

    }

    else

    {

      //compiled and linked in languages

      currentLanguagePtr = texts_all_languages;

      currentLanguageIndices = staticLanguageIndices[id];

      currentLanguageTypedText = typedTextDatabaseArray[id];

    }

  }

  if (currentLanguageTypedText)

  {

    currentLanguage = id;

    touchgfx::TypedText::registerTypedTextDatabase(currentLanguageTypedText,

                            TypedTextDatabase::getFonts(), TypedTextDatabase::getInstanceSize());

  }

}

void touchgfx::Texts::setTranslation(touchgfx::LanguageId id, const void* translation)

{

  languagesArray[id] = (const TranslationHeader*)translation;

}

const touchgfx::Unicode::UnicodeChar* touchgfx::Texts::getText(TypedTextId id) const

{

  return &currentLanguagePtr[currentLanguageIndices[id]];

}

STran.2
STran.2Author
Associate II
November 24, 2020

Enclosed is the full project for GFX version 4.13 (26.4 MB) This is the working version with lab4 completed.

STran.2
STran.2Author
Associate II
November 24, 2020

Enclosed is the full project for GFX version 4.14 up to the point after ToughGFX generated the code and STM32CubeIDE compile error. (40 MB) I am not sure why the compress files is so much larger for version 4.14.

STran.2
STran.2Author
Associate II
December 1, 2020

Hi Romain,

With respect to the problem I discovered and described previously, I think the TouchGFX 4.14.0 code generation for Texts.cpp file has problem. Will the TouchGFX team look into this issue and confirm my thoughts.

Regards,

Sy

FMarr.1
Associate II
December 12, 2020

Hi Stran.2,

did you solve the issue?

I have the same problem

STran.2
STran.2Author
Associate II
December 15, 2020

Hi FMarr

I down grade to ToughGFX 4.13 then it works as I show in the previous attachment. An ST employee has the suggested solution to use latest TouchGFX version here: STM32 Graphics Workshop - TouchGFX fail to run Target STM32H7B3I_DISCO

I have not try it yet but I will in a few weeks when I get back to working on STM project again. If you try the solution, please post if you have more information about it.

FMarr.1
Associate II
December 15, 2020

I did not try anymore to solve the error but I started a new project following the indication of the workshop with last firmware repository 1.08 , touchgfx 4.15 and idea 1.5 and it works. Cannot set the same clock setup.