Skip to main content
MŁask.1
Associate II
May 11, 2022 7:37 AM UTC
Question

LCD on nucleo STM32L073 doesn't initialize with contrast lower than 5.

When I set up contrast to value less than 5 I get stuck on HAL_LCD_Init() on wait for booster, and initialization fails:

 /*!< Wait Until the LCD Booster is ready */
 while(__HAL_LCD_GET_FLAG(hlcd, LCD_FLAG_RDY) == RESET)
 {
 if((HAL_GetTick() - tickstart ) > LCD_TIMEOUT_VALUE)
 { 
 hlcd->ErrorCode = HAL_LCD_ERROR_RDY;
 return HAL_TIMEOUT;
 } 
 }

Do I have to initilize something else to get other values of contrast?

 hlcd.Instance = LCD;
 hlcd.Init.Prescaler = LCD_PRESCALER_1;
 hlcd.Init.Divider = LCD_DIVIDER_31;
 hlcd.Init.Duty = LCD_DUTY_1_4;
 hlcd.Init.Bias = LCD_BIAS_1_3;
 hlcd.Init.VoltageSource = LCD_VOLTAGESOURCE_INTERNAL;
 hlcd.Init.Contrast = LCD_CONTRASTLEVEL_5;
 hlcd.Init.DeadTime = LCD_DEADTIME_0;
 hlcd.Init.PulseOnDuration = LCD_PULSEONDURATION_4;
 hlcd.Init.HighDrive = LCD_HIGHDRIVE_0;
 hlcd.Init.BlinkMode = LCD_BLINKMODE_OFF;
 hlcd.Init.BlinkFrequency = LCD_BLINKFREQUENCY_DIV8;
 hlcd.Init.MuxSegment = LCD_MUXSEGMENT_DISABLE;

This topic has been closed for replies.

1 reply

Visitor II
Mar 20, 2024 1:05 PM UTC

I al facing similar to above issue. I could not able to configure the internal voltage source. The while(__HAL_LCD_GET_FLAG(hlcd, LCD_FLAG_RDY) == RESET) never sets if the internal voltage source is selected. My configurations are listed below,

hlcd.Instance = LCD;

hlcd.Init.Prescaler = LCD_PRESCALER_1;

hlcd.Init.Divider = LCD_DIVIDER_31;

hlcd.Init.Duty = LCD_DUTY_1_4;

hlcd.Init.Bias = LCD_BIAS_1_3;

hlcd.Init.VoltageSource = LCD_VOLTAGESOURCE_INTERNAL;

hlcd.Init.Contrast = LCD_CONTRASTLEVEL_6;

hlcd.Init.DeadTime = LCD_DEADTIME_0;

hlcd.Init.PulseOnDuration = LCD_PULSEONDURATION_4;

hlcd.Init.HighDrive = LCD_HIGHDRIVE_0;

hlcd.Init.MuxSegment = LCD_MUXSEGMENT_DISABLE;

hlcd.Init.BlinkMode = LCD_BLINKMODE_OFF;

hlcd.Init.BlinkFrequency = LCD_BLINKFREQUENCY_DIV8;

 

Anybody faced similar issue. Anyone can support for solution