Skip to main content
Mna.1
Associate III
February 4, 2021
Question

LCD_CLK that runs XGA (1024 x 768)

  • February 4, 2021
  • 2 replies
  • 982 views

LCD_CLK that runs XGA (1024 x 768)

Thank you for helping.

environment:

STM32CubeIDE Ver1.5.0

MCU: STM32F769BI

Board: Custum

It seems that this microcomputer supports up to XGA, but LCD_CLK for XGA is not output.

Create LCD_CLK with PLL using a 25MHz crystal.

The XGA LCD panel is instructed to use a 65MHz clock with a Typ. Value.

If fps is 60 in XGA, I think that a clock of about 65MHz is required.

When I try to set 65MHz in the Clock configuration of the IDE, the output is DC.

I haven't looked at it in detail, but it seems to be output at around 10MHz or 30MHz.

GPIO_SPEED_FREQ_VERY_HIGH is selected as the GPIO speed.

How can I output a 65MHz LCD_CLK?

Also, what is the maximum frequency of LCD_CLK that can be output by STM32F769BI?

Thank you. 

This topic has been closed for replies.

2 replies

Tesla DeLorean
Guru
February 5, 2021

As I recall the DSI with a 16-bit colour depth would give the clock a ceiling of around 62.5 MHz, with 24-bit 41.67 MHz

I had 1024x768 running at 57 Hz and 51 Hz on the DSI/HDMI

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
Mna.1
Mna.1Author
Associate III
February 8, 2021

Hi Tesla DeLorean

Thank you for your reply.

In my case, I use RGB0-7, HSYNC, VSYNC, DE, LCD_CLK signals.

I would like to know the maximum frequency of LCD_CLK in this case.

Thank you.