[L0] LCD VLCD: wrong documentation and code generation
- 4 replies
- 2035 views
The datasheet (DS10685 Rev 6) in Table 16 says that the VLCD pins are:
PB0/LCD_VLCD3
PB2/LCD_VLCD2
PE11/LCD_VLCD1
PE12/LCD_VLCD3
PB12/LCD_VLCD1
In the reference manual RM0367 Rev 7 (for STM32L0x3)
Section 10.2.2 (SYSCFG_CFGR2), for bits LCD_CAPA:
Bit 1 controls the connection of VLCDrail1 on PB2/LCD_VLCD1
0: VLCDrail2 not connected to PB2/LCD_VLCD1
1: VLCDrail2 connected to PB2/LCD_VLCD1
Bit 2 controls the connection of VLCDrail1 on PB12
Bit 3 controls the connection of VLCDrail3 on PB0
Bit 4 controls the connection of VLCDrail1 on PE11
Bit 5 controls the connection of VLCDrail3 on PE12
So, the reference manual seems to be wrong about PB2.
The VLCD names are wrong in the schematics for STM32L073Z-EVAL too (document "MB1168.pdf" revision C-01): PB2 is marked as "VLCD1", and PE11 is marked as "VLCD2" (whereas PE12 is correctly marked as "VCLD3").
The actual voltages on the pins agree with the naming in the datasheet (PE11/LCD_VLCD1 < PB2/LCD_VLCD2 < PE12/LCD_VLCD3)
The options available in CubeMX fully agree with the datasheet (not the reference manual).
However, the code generation is partially wrong: the VLCD pins are properly configured as alternate-function GPIOs, but only some of them are also mentioned in the SYSCFG_CFGR2_LCDCAPA bits.
See the attached CubeMX project: in function MX_LCD_Init(), the following line is produced
__HAL_SYSCFG_VLCD_CAPA_CONFIG(SYSCFG_VLCD_PB0_EXT_CAPA_ON);
instead of
__HAL_SYSCFG_VLCD_CAPA_CONFIG(SYSCFG_VLCD_PB0_EXT_CAPA_ON|SYSCFG_VLCD_PB2_EXT_CAPA_ON|SYSCFG_VLCD_PE11_EXT_CAPA_ON);