Skip to main content
mAbul.1
Visitor II
Mar 21, 2020 3:02 PM UTC
Question

keil uVision5 can not compile generated code from TouchGFX 4.13.0. error is: can not finde include files. I am working on stm32f469i-DISCO board. when I searching those files. they are on the project folders.

..

This topic has been closed for replies.

3 replies

Martin KJELDSEN
Principal III
Mar 31, 2020 2:46 PM UTC

Please supply way more information to optimize chance of success.

One guess is that you might have forgotten to "generated code" from the designer.

/Martin

Tesla DeLorean
Guru
Mar 31, 2020 2:54 PM UTC

So find where the files are on your system, and add that path to the "Include Paths" so the compiler can find them too.

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
Martin KJELDSEN
Principal III
Mar 31, 2020 3:32 PM UTC

The project, when generated using CubeMX, is already set up to include the correct paths, but the "Generate code" from the designer is required in order to actually bootstrap the application with header files and libraries.

@mAbul.1​  - Tell me how you created the project and what your flow is like.

/Martin