Skip to main content
qbaj
Associate II
June 30, 2020
Question

JPEG - MDMA Write/Read Transfer Error

Hi,

I have error (Write/Read Transfer Error) when I'm using JPEG decoder via DMA

HAL_JPEG_Decode_DMA(hjpeg ,(uint8_t *)JPEGSourceAddress ,CHUNK_SIZE_IN ,(uint8_t *)FrameBufferAddress ,CHUNK_SIZE_OUT);

I don't get any interrupts from JPEG but from MDMA I get Transfer Error Interrupt:

- mdma_jpeg_in I get HAL_MDMA_ERROR_WRITE_XFER

hdma->Instance.CISR = 0x1
hdma->Instance.CESR = 0xC0
hdma->Instance.CSAR = 0x30000400
hdma->Instance.CDAR = 0x52003040

- mdma_jpeg_out I get HAL_MDMA_ERROR_READ_XFER

hdma->Instance.CISR = 0x1
hdma->Instance.CESR = 0x44
hdma->Instance.CSAR = 0x52003044
hdma->Instance.CDAR = 0x70119800

JPEGSourceAddress (0x30000400) in RAM_D2

FrameBufferAddress (0x70119800) in SD_RAM

HAL_JPEG_MspInit is copied from examples

 /* JPEG MDMA Init */
 /* JPEG_INFIFO_TH Init */
 hmdma_jpeg_in.Instance = MDMA_CHANNEL_JPEG_IN;
 hmdma_jpeg_in.Init.Request = MDMA_REQUEST_JPEG_INFIFO_TH;
 hmdma_jpeg_in.Init.TransferTriggerMode = MDMA_BUFFER_TRANSFER;
 hmdma_jpeg_in.Init.Priority = MDMA_PRIORITY_VERY_HIGH;
 hmdma_jpeg_in.Init.Endianness = MDMA_LITTLE_ENDIANNESS_PRESERVE;
 hmdma_jpeg_in.Init.SourceInc = MDMA_SRC_INC_BYTE;
 hmdma_jpeg_in.Init.DestinationInc = MDMA_DEST_INC_DISABLE;
 hmdma_jpeg_in.Init.SourceDataSize = MDMA_SRC_DATASIZE_BYTE;
 hmdma_jpeg_in.Init.DestDataSize = MDMA_DEST_DATASIZE_WORD;
 hmdma_jpeg_in.Init.DataAlignment = MDMA_DATAALIGN_PACKENABLE;
 hmdma_jpeg_in.Init.BufferTransferLength = 32;
 hmdma_jpeg_in.Init.SourceBurst = MDMA_SOURCE_BURST_32BEATS;
 hmdma_jpeg_in.Init.DestBurst = MDMA_DEST_BURST_16BEATS;
 hmdma_jpeg_in.Init.SourceBlockAddressOffset = 0;
 hmdma_jpeg_in.Init.DestBlockAddressOffset = 0;
 if (HAL_MDMA_Init(&hmdma_jpeg_in) != HAL_OK) {
 Error_Handler();
 }
 
 __HAL_LINKDMA(jpegHandle, hdmain, hmdma_jpeg_in);
 
 /* JPEG_OUTFIFO_TH Init */
 hmdma_jpeg_out.Instance = MDMA_CHANNEL_JPEG_OUT;
 hmdma_jpeg_out.Init.Request = MDMA_REQUEST_JPEG_OUTFIFO_TH;
 hmdma_jpeg_out.Init.TransferTriggerMode = MDMA_BUFFER_TRANSFER;
 hmdma_jpeg_out.Init.Priority = MDMA_PRIORITY_VERY_HIGH;
 hmdma_jpeg_out.Init.Endianness = MDMA_LITTLE_ENDIANNESS_PRESERVE;
 hmdma_jpeg_out.Init.SourceInc = MDMA_SRC_INC_DISABLE;
 hmdma_jpeg_out.Init.DestinationInc = MDMA_DEST_INC_BYTE;
 hmdma_jpeg_out.Init.SourceDataSize = MDMA_SRC_DATASIZE_WORD;
 hmdma_jpeg_out.Init.DestDataSize = MDMA_DEST_DATASIZE_BYTE;
 hmdma_jpeg_out.Init.DataAlignment = MDMA_DATAALIGN_PACKENABLE;
 hmdma_jpeg_out.Init.BufferTransferLength = 32;
 hmdma_jpeg_out.Init.SourceBurst = MDMA_SOURCE_BURST_32BEATS;
 hmdma_jpeg_out.Init.DestBurst = MDMA_DEST_BURST_32BEATS;
 hmdma_jpeg_out.Init.SourceBlockAddressOffset = 0;
 hmdma_jpeg_out.Init.DestBlockAddressOffset = 0;
 if (HAL_MDMA_Init(&hmdma_jpeg_out) != HAL_OK) {
 Error_Handler();
 }

Why MDMA has no access to JPEG registers?

This topic has been closed for replies.