Skip to main content
VDuch.11
Associate II
October 9, 2020
Question

It would be nice to have support for the STM32F413 disco board

Hello, I recently bought one STM32F413Discovery board, and I would like to ask the developers to create a TouchGFX example in order to use also the display with the new software, and not using the old STemWin.

Thank you

This topic has been closed for replies.

2 replies

ST Technical Moderator
October 9, 2020

Hello @VDuch.1​ ,

Thank you for your feedback. I will raise you request internally regarding TouchGFX example for STM32F413-Disco.

I suggest that you have a look on the TouchGFX demo and get inspired from them:

  • STM32Cube_FW_F4_V1.25.1\Projects\STM32F429I-Discovery\Demonstrations\TouchGFX\
  • STM32Cube_FW_F4_V1.25.1\Projects\STM32469I_EVAL\Demonstrations\TouchGFX\

You can refer to the TouchGFX User guide, TouchGFX User manual and TouchGFX MOOC, this will help you to create your STM32 based application using TouchGFX and STM32CubeIDE.

Please let me know if this support has been useful to you.

Imen

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Thanks
ST Technical Moderator
October 13, 2020

Hi @VDuch.1​ ,

I've heard back from the TouchGFX team and at the moment, there is no short term plan to add TouchGFX example for STM32F413Discovery board.

There’s an application template for STM32F412 within STM32CubeF4 that you can run our UI templates (examples) on.

I hope that this example is useful for you.

Imen

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Thanks