Skip to main content
Associate II
Feb 21, 2025 7:45 PM UTC
Solved

It is possible to pass a value from view to container

Hello.

I have a project on TouchGFX Designer, in a view (called routing_channel) i have a ScrollList with a container that i use as template.

I am doing the scroll with hardware buttons, my goal is, get the index value from the items of the list and pass this value to container.

How can i pass values from view to container? 

example:

ScrollList
item1
item2 < Selected this item, now i want to pass his index value to the container
item3

If my goal isn't clear enough, i can provide more details. Thanks!

    This topic has been closed for replies.
    matheuschiarelliBest answer
    Associate II
    Mar 5, 2025 11:54 AM UTC

    Hello, @LouisB 

    Actually i solved the problem by following this other topic. My problem was with the list update function, same as the topic's question.

    https://community.st.com/t5/stm32-mcus-touchgfx-and-gui/touchgfx-scroll-list-invalidate-problem-stm32h750b-dk/m-p/687465#M38158

    Sorry for any inconvenience.

    4 replies

    ST Employee
    Feb 24, 2025 8:32 AM UTC

    Hello @matheuschiarelli,

    When you say "scroll with hardware buttons", it means that, you go from one item to another by using buttons or the scroll itself is done by buttons ?

    If that's the first case with a scroll list, one solution is to keep track of the current element by using a cursor that you increment and decrement each time the button is clicked. You can use "animateToItem" like:

     

     

    ...
    void MyScreen::buttonUp()
    {
     if(cursor < MAXCURSOR)
     {
     cursor ++;
     scrollList1.animateToItem(cursor);
     #DO_MY_THING_WITH_CONTAINER
     }
    }
    ...

     

     

    I hope it helps,
    BR,

    Louis BOUDOST Software Engineer | TouchGFX
    Associate II
    Feb 24, 2025 11:05 AM UTC

    Hello @LouisB 

    Actually, the scroll itself is done by buttons. To be more specific in my goal: I have some Flex Buttons in container that i want to change their value (from "released" to "pressed" for example) by sending boolean value from view to container. I mentioned the scroll because my display doesn't have touch, so i need to get the scroll item's value by hardware button (if is possible).

    I was trying this:

    //Function example in container
    void RoutingContainer::setButtonState(bool pressed)
    {
     btn_left.setPressed(pressed);
     btn_left.invalidate();
    }

     

    //Function example in view
    
    void routing_channelView::sendValueToContainer(RoutingContainer& item)
    {
    	item.setButtonState(true);
    }

    . 

    ST Employee
    Mar 4, 2025 2:16 PM UTC

    Hello @matheuschiarelli ,

    I saw that you create this thread Update flex button from a view to custom container - STMicroelectronics Community for the same issue. Please don't do duplicated thread for the same question.

    There's some things I don't understand, which function is called when you click ? and how do you know which element is the current one ? You can also check the example in Designer and draw inspiration from it.

    BR,

    Louis BOUDOST Software Engineer | TouchGFX
    matheuschiarelliAuthorBest answer
    Associate II
    Mar 5, 2025 11:54 AM UTC

    Hello, @LouisB 

    Actually i solved the problem by following this other topic. My problem was with the list update function, same as the topic's question.

    https://community.st.com/t5/stm32-mcus-touchgfx-and-gui/touchgfx-scroll-list-invalidate-problem-stm32h750b-dk/m-p/687465#M38158

    Sorry for any inconvenience.