Skip to main content
PBU
Associate III
Jul 23, 2019 12:00 PM UTC
Question

Issue in Porting from STM32F7 to STM32H7

Hi,

I'm trying to port code from STM32F7 series controller to STM32H7 controller. The code is working fine with STm32F7 (TouchFX + FreeRTOS). But in STM32H7 i am getting LTDC AHB Bus transfer error. I'm running only GUI Task and initialized the required peripherals like LTDC, FMC. Also Using HAL, Instrumentation, and DMA files generated by touchgfx designer for H750 board. My problem is task is running once and suddenly it get locked into LTDC_ER_IRQHandler. I have verified LTDC and FMC and it is working properly without using touchgfx.

This topic has been closed for replies.

4 replies

Tesla DeLorean
Guru
Jul 23, 2019 12:08 PM UTC

Check memory region usage. The H7 has many different rules and limitations about what can connect to what. Check bus matrix diagrams in RM

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
PBU
PBUAuthor
Associate III
Jul 23, 2019 3:21 PM UTC

Hi @Community member​ 

I am placing frame buffer in external SDRAM, also verified bus matrix diagrams in RM that whether LTDC, DMA2D is connected with FMC. Still facing the same issue.

Tesla DeLorean
Guru
Jul 23, 2019 3:27 PM UTC

Things will get stuck in IRQHandlers when the causing event doesn't actually get clearer, and it will infinitely tail-chain. Or if the event triggers at a rate which saturates the system.

Probably should look critically at what is enabled, and what is flagging. And any error statuses are being thrown off by the hardware side.

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
PBU
PBUAuthor
Associate III
Jul 24, 2019 5:29 AM UTC

Hi @Community member​ 

Thank you for the reply. The issue is DMA2D interrupt was mot handled properly. Now it is working fine.