Skip to main content
a_niedworok2
Associate II
Jun 30, 2025 9:27 PM UTC
Solved

Is X-NUCLEO-GFX01M2 compatible with NUCLEO-H533RE ?

Hello!

I wanted to ask if theX-NUCLEO-GFX01M2 module is compatible with STM32 NUCLEO-H533RE? The official documentation does not say anything about this NUCLEO board.

Kind regards 

Andrew 

This topic has been closed for replies.
Osman SOYKURT
Osman SOYKURTBest answer
ST Technical Moderator
Jul 3, 2025 8:18 AM UTC

Hello @a_niedworok2 ,

Yes this X-NUCLEO-GFX01M2 shield is compatible with STM32 NUCLEO-H533RE.

ST Software Developer | TouchGFX

3 replies

Osman SOYKURT
Osman SOYKURTBest answer
ST Technical Moderator
Jul 3, 2025 8:18 AM UTC

Hello @a_niedworok2 ,

Yes this X-NUCLEO-GFX01M2 shield is compatible with STM32 NUCLEO-H533RE.

ST Software Developer | TouchGFX
a_niedworok2
Associate II
Jul 5, 2025 4:27 PM UTC

Thank you for the information.

Is there a driver available for this LCD for the H533?

Andrew

Osman SOYKURT
ST Technical Moderator
Jul 9, 2025 10:46 AM UTC

The display driver is the same as the other small NUCLEO TBSs (like the NUCLEO-G071RB TBS for instance).
However, if you intend to use the external flash (the one in the display shield), then you would need to create an external loader and use it when flashing your board.

ST Software Developer | TouchGFX