Skip to main content
Louis Cloete work
Associate III
Sep 26, 2022 11:00 AM UTC
Question

Is TouchGFX GUI with Bridgetek FT81x graphics co-processor possible? Already available?

I'm in the process of evaluating options for a 5" display. We're looking at using the FT81x controller with lvgl or TouchGFX. I want to find out if TouchGFX can be used to drive the FT81x chip.

I do know lvgl can do something along those lines, but we have knowledge of TouchGFX in-house (used in personal hobby projects). If we can use the FT81x with a L4 series microcontroller and TouchGFX it would be ideal.

Do libraries exist to marry TouchGFX with the FT81x chips? Is it possible to write code to do that in a relatively short time if not?

This topic has been closed for replies.