Skip to main content
Associate III
Jul 12, 2023 7:44 AM UTC
Solved

Is Tilting the Image is possible in TouchGFX?

Hii,

I am selecting the STM32F746G Discovery Board in TouchGFX Designer. In the Designer I have taken a Tiled image widget and I am trying to move the image vertically up and down. Now I want the same image to be tilted with some angle in TouchGFX. Is that possible?

If it is, then how it works?

This topic has been closed for replies.
Yoann KLEIN
Yoann KLEINBest answer
ST Employee
Jul 12, 2023 2:08 PM UTC

Hello @Shivani,

Yes that's definitely doable, and quite easy to implement with a TextureMapper.

This widget allows the user to flip, rotate or scale the image with different angles.

 

Let me know if you have more questions.

Yoann KLEINST Software Developer | TouchGFX

4 replies

Yoann KLEIN
Yoann KLEINBest answer
ST Employee
Jul 12, 2023 2:08 PM UTC

Hello @Shivani,

Yes that's definitely doable, and quite easy to implement with a TextureMapper.

This widget allows the user to flip, rotate or scale the image with different angles.

 

Let me know if you have more questions.

Yoann KLEINST Software Developer | TouchGFX
ShivaniAuthor
Associate III
Jul 13, 2023 11:35 AM UTC

Hello @Shivani

I have implemented with TextureMapper, and it works fine...

Thank you...

ShivaniAuthor
Associate III
Feb 17, 2024 4:59 AM UTC

Hii .@Yoann KLEIN,

Is it possible to rotate the box or any  other widget from the TouchGFX Designer rather than using the TextureMapper?

Because I don't want to flip or rotate the image. 

If it is, then how it works?

How to rotate the widget both clockwise and anticlockwise?