Skip to main content
SWall.2
Associate III
December 10, 2020
Question

Is there a soldered connection to be made on the STM32L476VG microcontroller to enable the LCD display?

I have installed the example software for the STM32L476VG microcontrooller for the audio recorder.The HAL driver files for the LCD screen has been installed also.The LCD screen wont enable.Is there a soldered connection on the bottom of the PCB board or something that can be done to get the display to operate?

This topic has been closed for replies.

1 reply

Tesla DeLorean
Guru
December 10, 2020

The STM32L476G-DISCO?

Not a board I have to hand, but seem to recollect the demo working out of the box?

The schematic/user manual should enumerate the solder bridges, and the README files frequently call out specific requirements/expectations.

Try the example, uses the display at some point, and measures current, etc.

STM32Cube_FW_L4_V1.14.0\Projects\32L476GDISCOVERY\Examples\BSP

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..