Skip to main content
John Chinnick
Visitor II
Oct 16, 2018 3:26 PM UTC
Question

Is there a plan to add emWinSPY support to STemWin for the STM32F7 family of embedded processors?

When I look at the object dump of STemWin540_M7_OS_GCC_ARGB.lib I cannot find the GUI_SPY_Process function that is required by the server application to export the SPY data from the embedded target.

I do see the module included in the STemWin540_WIN32.lib, which allows monitoring in the simulator.

This topic has been closed for replies.