Skip to main content
FDi I
Associate
Jul 12, 2019 1:10 PM UTC
Question

Is there a *.ioc file configured for the STM32469I-EVAL and STM32479I-EVAL boards?

I created a new project with STM32CubeIDE (v1.00 or v1.01) choosing an STM32469I-EVAL or STM32479I-EVAL board, but the Device Configurator creates an empty ioc file.

They are a weel known evaluation boards, so I expect that ST can provide a valid *.ioc file with TouchGFX enabled.

This topic has been closed for replies.

3 replies

Tesla DeLorean
Guru
Jul 12, 2019 5:04 PM UTC

ST moves in mysterious and mercurial ways, press your sales, and FAE contacts with your support expectations.

@Martin KJELDSEN​  has posted template/rough-framed IOC files previously for assorted boards using the TouchGFX framework.

@Markus GIRDLAND​  has handled serviceability issues with the STM32CubeIDE line.

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
Markus GIRDLAND
ST Employee
Jul 15, 2019 10:02 AM UTC

What exactly do you mean by "an empty ioc file"? It's just blank white nothingness when you open the .ioc file inside CubeIDE?

I just created one of each for both EVAL boards and it seems to create a working .ioc for me. Or do you mean some specific function missing?

FDi I
FDi IAuthor
Associate
Jul 22, 2019 1:56 PM UTC

Dear @Markus GIRDLAND​ and @Community member​ ,

thanks for the quick answere.

Please, find in attachment the screenshots of the ioc file, all the middleware are not configured.

I have used the STM32CubeIDE v1.0.1 for the board STM32479I-EVAL.

Thanks.

BR, Felice