Skip to main content
YJMoon
Associate III
August 19, 2020
Solved

Is the development environment of STM32H7 & TouchGFX similar to STM32F7?

Hello.

I was developing a GUI with STM32F767 & RGB TFT LCD.

However, the specification has changed and I should consider changing to the STM32H743.

Are there any issues to watch out for when changing the cpu?

Does CubeIDE & TouchGFX Deginer support H7 development environment?

If yes, which version can I use?

​

Thanks for your help.

This topic has been closed for replies.
Romain DIELEMAN
Romain DIELEMANBest answer
ST Employee
August 19, 2020

Hi,

TouchGFX does support H7 development. There is an application template within Designer for the H743 eval board, you can have a look at it and get some inspiration to set up your configuration.

Concerning potential issues when changing cpus, I don't know sorry :beaming_face_with_smiling_eyes:.

/Romain

3 replies

Romain DIELEMAN
Romain DIELEMANBest answer
ST Employee
August 19, 2020

Hi,

TouchGFX does support H7 development. There is an application template within Designer for the H743 eval board, you can have a look at it and get some inspiration to set up your configuration.

Concerning potential issues when changing cpus, I don't know sorry :beaming_face_with_smiling_eyes:.

/Romain

YJMoon
YJMoonAuthor
Associate III
August 19, 2020

Thanks for your answer. It’s a good thing TouchGFX supports H7.

Have a nice day!

/YMoon

Romain DIELEMAN
ST Employee
August 19, 2020

Thanks, you too ^^