Skip to main content
RBurg.2
Associate III
May 21, 2021
Question

Is ST EEPROM emulation possible while touchgfx is running.

Hi, I am trying to use the ST-CUBE-EEPROM driver to store some settings with touchgfx 4.16.

I have a separate section defined in the linker script, 24kB for 500 variables at the end of the internal flash. It works well if I run it before the touchgfx task starts.

If I try to read a variable while touchgfx task is running I get a WRPERR in the flash status register. I have image assets stored in memory mapped external flash and fonts in internal flash. Am I able to stop touchgfx from locking the section I defined for the EEPROM somehow? Or do I have to go down the same route as suggested for memory mapped external flash by stopping the touchgfx task?

Thanks for the help :)

Russell Burge

This topic has been closed for replies.

2 replies

Tesla DeLorean
Guru
May 21, 2021

The internal flash introduces significant stalling issues during write/erase, so highly problematic for real-time work

A structure and direct use of flash is recommended over the eprom emulation

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
Piranha
Principal III
May 22, 2021

Stalling can be really long and a serious issue while erasing. When writing it is typically at a microsecond range and can be tolerated in many projects. Reading should "just work". If it causes a write protection error like WRPERR, there definitely is a bug somewhere.